![]() |
![]() |
I2S Hardware attributes. More...
#include <I2SCC26XX.h>
Data Fields | |
uint_least8_t | pinSD1 |
uint_least8_t | pinSD0 |
uint_least8_t | pinSCK |
uint_least8_t | pinCCLK |
uint_least8_t | pinWS |
uint8_t | intPriority |
I2S Hardware attributes.
intPriority is the I2S peripheral's interrupt priority, as defined by the RTOS kernel. This value is passed unmodified to HwiP_construct().
pinSD1 and pinSD0 define the SD0 and SD1 data pin mapping, respectively. pinSCK, pinCCLK and pinWS define the SCK, CCLK and WS clock pin mapping, respectively. All these pins are typically defined with a macro in a header file, which maps to an IOID.
A sample structure is shown below:
uint_least8_t I2SCC26XX_HWAttrs::pinSD1 |
Pin used for SD1 signal.
uint_least8_t I2SCC26XX_HWAttrs::pinSD0 |
Pin used for SD0 signal.
uint_least8_t I2SCC26XX_HWAttrs::pinSCK |
Pin used for SCK signal.
uint_least8_t I2SCC26XX_HWAttrs::pinCCLK |
Pin used for CCLK signal. Not used in most of the applications.
uint_least8_t I2SCC26XX_HWAttrs::pinWS |
Pin used for WS signal.
uint8_t I2SCC26XX_HWAttrs::intPriority |
I2S Peripheral's interrupt priority.