Functions
PowerCC26X2_helpers.h File Reference
#include <string.h>
Include dependency graph for PowerCC26X2_helpers.h:

Go to the source code of this file.

Functions

void PowerCC26X2_oscCtlClearXtal (void)
 
void PowerCC26X2_pmctlDisableJtag (void)
 
void PowerCC26X2_sysctrlShutdownWithAbort (void)
 
void PowerCC26X2_prcmEnableCacheRetention (void)
 
void PowerCC26X2_oschfSwitchToRcosc (void)
 
uint32_t PowerCC26X2_oscClockSourceGet (uint32_t ui32SrcClk)
 
void PowerCC26X2_oscDisableQualifiers (void)
 
bool PowerCC26X2_getOscHfSourceReady (void)
 
uint32_t PowerCC26X2_oschfTrySwitchToXosc (void)
 
bool PowerCC26X2_oscIsHPOSCEnabledWithHfDerivedLfClock (void)
 
void PowerCC26X2_enableTCXOQual (void)
 
void PowerCC26X2_disableTCXOQual (void)
 
void PowerCC26X2_switchToTCXO (void)
 
void PowerCC26X2_turnOnXosc (void)
 
void PowerCC26X2_sysCtrlStandby (bool retainCache)
 
void PowerCC26X2_sysCtrlVoltageConditionalControl (void)
 
void PowerCC26X2_sysCtrlIdle (uint32_t vimsPdMode)
 
void PowerCC26X2_setPeriphDependency (uint32_t prcmPeriph)
 
void PowerCC26X2_releasePeriphDependency (uint32_t prcmPeriph)
 
void PowerCC26X2_setPeriphDeepSleepEnable (uint32_t prcmPeriph)
 
uint32_t PowerCC26X2_sysCtrlGetResetSource (void)
 
void PowerCC26X2_setSubSecIncToXoscLf (uint32_t subsecinc)
 
void PowerCC26X2_sysCtrlUpdateVoltageRegulator (void)
 
void PowerCC26X2_sysCtrlReset (void)
 
void PowerCC26X2_updateSubSecInc (bool firstLF)
 
int32_t PowerCC26X2_readCtrim (void)
 
int32_t PowerCC26X2_readCtrimFract (void)
 
int32_t PowerCC26X2_readRtrim (void)
 
void PowerCC26X2_writeCtrim (int32_t newValue)
 
void PowerCC26X2_writeCtrimFract (int32_t newValue)
 
void PowerCC26X2_writeCtrimFractEn (int32_t newValue)
 
void PowerCC26X2_writeRtrim (int32_t newValue)
 
void PowerCC26X2_setTdcClkSrc24M (void)
 
void PowerCC26X2_setAclkRefSrc (uint32_t source)
 

Function Documentation

§ PowerCC26X2_oscCtlClearXtal()

void PowerCC26X2_oscCtlClearXtal ( void  )

§ PowerCC26X2_pmctlDisableJtag()

void PowerCC26X2_pmctlDisableJtag ( void  )

§ PowerCC26X2_sysctrlShutdownWithAbort()

void PowerCC26X2_sysctrlShutdownWithAbort ( void  )

§ PowerCC26X2_prcmEnableCacheRetention()

void PowerCC26X2_prcmEnableCacheRetention ( void  )

§ PowerCC26X2_oschfSwitchToRcosc()

void PowerCC26X2_oschfSwitchToRcosc ( void  )

§ PowerCC26X2_oscClockSourceGet()

uint32_t PowerCC26X2_oscClockSourceGet ( uint32_t  ui32SrcClk)

§ PowerCC26X2_oscDisableQualifiers()

void PowerCC26X2_oscDisableQualifiers ( void  )

§ PowerCC26X2_getOscHfSourceReady()

bool PowerCC26X2_getOscHfSourceReady ( void  )

§ PowerCC26X2_oschfTrySwitchToXosc()

uint32_t PowerCC26X2_oschfTrySwitchToXosc ( void  )

§ PowerCC26X2_oscIsHPOSCEnabledWithHfDerivedLfClock()

bool PowerCC26X2_oscIsHPOSCEnabledWithHfDerivedLfClock ( void  )

§ PowerCC26X2_enableTCXOQual()

void PowerCC26X2_enableTCXOQual ( void  )

§ PowerCC26X2_disableTCXOQual()

void PowerCC26X2_disableTCXOQual ( void  )

§ PowerCC26X2_switchToTCXO()

void PowerCC26X2_switchToTCXO ( void  )

§ PowerCC26X2_turnOnXosc()

void PowerCC26X2_turnOnXosc ( void  )

§ PowerCC26X2_sysCtrlStandby()

void PowerCC26X2_sysCtrlStandby ( bool  retainCache)

§ PowerCC26X2_sysCtrlVoltageConditionalControl()

void PowerCC26X2_sysCtrlVoltageConditionalControl ( void  )

§ PowerCC26X2_sysCtrlIdle()

void PowerCC26X2_sysCtrlIdle ( uint32_t  vimsPdMode)

§ PowerCC26X2_setPeriphDependency()

void PowerCC26X2_setPeriphDependency ( uint32_t  prcmPeriph)

§ PowerCC26X2_releasePeriphDependency()

void PowerCC26X2_releasePeriphDependency ( uint32_t  prcmPeriph)

§ PowerCC26X2_setPeriphDeepSleepEnable()

void PowerCC26X2_setPeriphDeepSleepEnable ( uint32_t  prcmPeriph)

§ PowerCC26X2_sysCtrlGetResetSource()

uint32_t PowerCC26X2_sysCtrlGetResetSource ( void  )

§ PowerCC26X2_setSubSecIncToXoscLf()

void PowerCC26X2_setSubSecIncToXoscLf ( uint32_t  subsecinc)

§ PowerCC26X2_sysCtrlUpdateVoltageRegulator()

void PowerCC26X2_sysCtrlUpdateVoltageRegulator ( void  )

§ PowerCC26X2_sysCtrlReset()

void PowerCC26X2_sysCtrlReset ( void  )

§ PowerCC26X2_updateSubSecInc()

void PowerCC26X2_updateSubSecInc ( bool  firstLF)

§ PowerCC26X2_readCtrim()

int32_t PowerCC26X2_readCtrim ( void  )

§ PowerCC26X2_readCtrimFract()

int32_t PowerCC26X2_readCtrimFract ( void  )

§ PowerCC26X2_readRtrim()

int32_t PowerCC26X2_readRtrim ( void  )

§ PowerCC26X2_writeCtrim()

void PowerCC26X2_writeCtrim ( int32_t  newValue)

§ PowerCC26X2_writeCtrimFract()

void PowerCC26X2_writeCtrimFract ( int32_t  newValue)

§ PowerCC26X2_writeCtrimFractEn()

void PowerCC26X2_writeCtrimFractEn ( int32_t  newValue)

§ PowerCC26X2_writeRtrim()

void PowerCC26X2_writeRtrim ( int32_t  newValue)

§ PowerCC26X2_setTdcClkSrc24M()

void PowerCC26X2_setTdcClkSrc24M ( void  )

§ PowerCC26X2_setAclkRefSrc()

void PowerCC26X2_setAclkRefSrc ( uint32_t  source)
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale