ECJPAKECC26X2.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2017-2023, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
88 #ifndef ti_drivers_ecjpake_ECJPAKECC26X2__include
89 #define ti_drivers_ecjpake_ECJPAKECC26X2__include
90 
91 #include <stdint.h>
92 #include <stdbool.h>
93 
94 #include <ti/drivers/ECJPAKE.h>
95 
96 #ifdef __cplusplus
97 extern "C" {
98 #endif
99 
100 /* Exit the SWI and wait until an HWI call posts the SWI again */
101 #define ECJPAKECC26X2_STATUS_FSM_RUN_PKA_OP ECJPAKE_STATUS_RESERVED - 0
102 /* Execute the next FSM state immediately without waiting for the next HWI */
103 #define ECJPAKECC26X2_STATUS_FSM_RUN_FSM ECJPAKE_STATUS_RESERVED - 1
104 
114 typedef enum
115 {
126 
138 
149 
165 
175 
177 
184 typedef struct
185 {
199  uint8_t intPriority;
201 
207 typedef struct
208 {
209  bool isOpen;
212  int_fast16_t operationStatus;
215  ECJPAKECC26X2_FsmState fsmState;
219  uint32_t resultAddress;
221 
222 #ifdef __cplusplus
223 }
224 #endif
225 
226 #endif /* ti_drivers_ecjpake_ECJPAKECC26X2__include */
Definition: ECJPAKECC26X2.h:140
Definition: ECJPAKECC26X2.h:141
Definition: ECJPAKECC26X2.h:142
ECJPAKE_OperationType
Enum for the operation types supported by the driver.
Definition: ECJPAKE.h:1118
ECJPAKECC26X2_FsmState fsmState
Definition: ECJPAKECC26X2.h:215
Definition: ECJPAKECC26X2.h:146
bool isOpen
Definition: ECJPAKECC26X2.h:209
int_fast16_t operationStatus
Definition: ECJPAKECC26X2.h:212
ECJPAKE_ReturnBehavior returnBehavior
Definition: ECJPAKECC26X2.h:214
uint8_t intPriority
PKA Peripheral&#39;s interrupt priority.
Definition: ECJPAKECC26X2.h:199
void(* ECJPAKE_CallbackFxn)(ECJPAKE_Handle handle, int_fast16_t returnStatus, ECJPAKE_Operation operation, ECJPAKE_OperationType operationType)
The definition of a callback function used by the ECJPAKE driver when used in ECJPAKE_RETURN_BEHAVIOR...
Definition: ECJPAKE.h:1145
Definition: ECJPAKECC26X2.h:144
bool operationInProgress
Definition: ECJPAKECC26X2.h:210
Definition: ECJPAKECC26X2.h:131
ECJPAKECC26X2 Object.
Definition: ECJPAKECC26X2.h:207
Definition: ECJPAKECC26X2.h:116
uint32_t resultAddress
Definition: ECJPAKECC26X2.h:219
uint32_t semaphoreTimeout
Definition: ECJPAKECC26X2.h:218
Definition: ECJPAKECC26X2.h:137
ECJPAKECC26X2_FsmState
ECJPAKECC26X2 states.
Definition: ECJPAKECC26X2.h:114
Definition: ECJPAKECC26X2.h:158
Definition: ECJPAKECC26X2.h:148
ECJPAKECC26X2 Hardware Attributes.
Definition: ECJPAKECC26X2.h:184
TI Driver for Elliptic Curve Password Authenticated Key Exchange by Juggling.
Definition: ECJPAKECC26X2.h:164
bool operationCanceled
Definition: ECJPAKECC26X2.h:211
ECJPAKE_Operation operation
Definition: ECJPAKECC26X2.h:216
Definition: ECJPAKECC26X2.h:125
ECJPAKE_ReturnBehavior
The way in which ECJPAKE function calls return after performing an encryption + authentication or dec...
Definition: ECJPAKE.h:861
ECJPAKE_CallbackFxn callbackFxn
Definition: ECJPAKECC26X2.h:213
Definition: ECJPAKECC26X2.h:162
ECJPAKE_OperationType operationType
Definition: ECJPAKECC26X2.h:217
Union containing pointers to all supported operation structs.
Definition: ECJPAKE.h:1103
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale