Enumerations | Functions | Variables
CryptoUtils.h File Reference

Detailed Description

A collection of utility functions for cryptographic purposes.

============================================================================

#include <stdint.h>
#include <stdbool.h>
#include <string.h>
Include dependency graph for CryptoUtils.h:

Go to the source code of this file.

Enumerations

enum  CryptoUtils_Endianess { CryptoUtils_ENDIANESS_BIG = 0u, CryptoUtils_ENDIANESS_LITTLE = 1u }
 Indicates the endianess (byte order) of a multi-byte value. More...
 

Functions

bool CryptoUtils_buffersMatch (const volatile void *volatile buffer0, const volatile void *volatile buffer1, size_t bufferByteLength)
 Compares two buffers for equality without branching. More...
 
bool CryptoUtils_buffersMatchWordAligned (const volatile uint32_t *volatile buffer0, const volatile uint32_t *volatile buffer1, size_t bufferByteLength)
 Compares two buffers for equality word-by-word without branching. More...
 
bool CryptoUtils_isBufferAllZeros (const void *buffer, size_t bufferByteLength)
 Check whether the provided buffer only contains 0x00 bytes. More...
 
void CryptoUtils_memset (void *dest, size_t destSize, uint8_t val, size_t count)
 Copies val into the first count bytes of the buffer pointed to by dest. More...
 
void CryptoUtils_reverseBufferBytewise (void *buffer, size_t bufferByteLength)
 Reverses the byte order in a buffer of a given length. More...
 
void CryptoUtils_copyPad (const void *source, uint32_t *destination, size_t sourceLength)
 Copies and pads an array of words. More...
 
void CryptoUtils_reverseCopyPad (const void *source, uint32_t *destination, size_t sourceLength)
 Reverses, copies, and pads an array of words. More...
 
void CryptoUtils_reverseCopy (const void *source, void *destination, size_t sourceLength)
 Reverses and copies an array of bytes. More...
 
bool CryptoUtils_isNumberInRange (const void *number, size_t bitLength, CryptoUtils_Endianess endianess, const void *lowerLimit, const void *upperLimit)
 Checks if number is within the range [lowerLimit, upperLimit) More...
 

Variables

const uint8_t * CryptoUtils_limitZero
 Limit value of 0. More...
 
const uint8_t * CryptoUtils_limitOne
 Limit value of 1. More...
 

Enumeration Type Documentation

§ CryptoUtils_Endianess

Indicates the endianess (byte order) of a multi-byte value.

Enumerator
CryptoUtils_ENDIANESS_BIG 

MSB at lowest address.

CryptoUtils_ENDIANESS_LITTLE 

LSB at highest address.

Function Documentation

§ CryptoUtils_buffersMatch()

bool CryptoUtils_buffersMatch ( const volatile void *volatile  buffer0,
const volatile void *volatile  buffer1,
size_t  bufferByteLength 
)

Compares two buffers for equality without branching.

Note
This is not a drop-in replacement for memcmp!

Most memcmp implementations break out of their comparison loop immediately once a mismatch is detected to save execution time. For cryptographic purposes, this is a flaw.

This function compares two buffers without branching thus requiring a an amount of time that does not vary with the content of buffer0 and buffer1.

Parameters
buffer0Buffer to compare against buffer1.
buffer1Buffer tp compare against buffer0
bufferByteLengthLength in bytes of buffer0 and buffer1.
Return values
trueThe contents of the buffers match.
falseThe contents of the buffers do not match.

§ CryptoUtils_buffersMatchWordAligned()

bool CryptoUtils_buffersMatchWordAligned ( const volatile uint32_t *volatile  buffer0,
const volatile uint32_t *volatile  buffer1,
size_t  bufferByteLength 
)

Compares two buffers for equality word-by-word without branching.

Note
This is not a drop-in replacement for memcmp!

Most memcmp implementations break out of their comparison loop immediately once a mismatch is detected to save execution time. For cryptographic purposes, this is a flaw.

This function compares two buffers without branching thus requiring a an amount of time that does not vary with the content of buffer0 and buffer1.

Unlike CryptoUtils_buffersMatch(), this function expects buffer0 and buffer1 to be 32-bit aligned. It will only perform 32-bit aligned accesses to memory. This is needed to access the registers of certain peripherals.

Parameters
buffer0Buffer to compare against buffer1.
buffer1Buffer tp compare against buffer0
bufferByteLengthLength in bytes of buffer0 and buffer1. Must be evenly divisible by sizeof(uint32_t). This function will return false if bufferByteLength is not evenly divisible by sizeof(uin32_t).
Return values
trueThe contents of the buffers match.
falseThe contents of the buffers do not match.

§ CryptoUtils_isBufferAllZeros()

bool CryptoUtils_isBufferAllZeros ( const void *  buffer,
size_t  bufferByteLength 
)

Check whether the provided buffer only contains 0x00 bytes.

Parameters
bufferBuffer to search for non-zero bytes
bufferByteLengthLength of buffer in bytes
Return values
trueThe buffer contained only bytes with value 0x00
falseThe buffer contained at least one non-zero byte

§ CryptoUtils_memset()

void CryptoUtils_memset ( void *  dest,
size_t  destSize,
uint8_t  val,
size_t  count 
)

Copies val into the first count bytes of the buffer pointed to by dest.

Parameters
destPointer to destination buffer
destSizeSize of destination buffer in bytes
valFill byte value
countNumber of bytes to fill

§ CryptoUtils_reverseBufferBytewise()

void CryptoUtils_reverseBufferBytewise ( void *  buffer,
size_t  bufferByteLength 
)

Reverses the byte order in a buffer of a given length.

The left-most byte will become the right-most byte and vice versa.

Parameters
bufferBuffer containing the data to be reversed.
bufferByteLengthLength in bytes of buffer.

§ CryptoUtils_copyPad()

void CryptoUtils_copyPad ( const void *  source,
uint32_t *  destination,
size_t  sourceLength 
)

Copies and pads an array of words.

The source array is copied into the destination array. Writes are done word-wise. If sourceLength is not a multiple of 4, any remaining bytes up to the next word boundary are padded with 0.

The length of the destination array must be a multiple of 4, rounded up to the padded sourceLength if required.

Parameters
sourceSource array
destinationDestination array
sourceLengthLength of the source array

§ CryptoUtils_reverseCopyPad()

void CryptoUtils_reverseCopyPad ( const void *  source,
uint32_t *  destination,
size_t  sourceLength 
)

Reverses, copies, and pads an array of words.

The source array is reversed byte-wise and copied into the destination array. Writes are done word-wise. If sourceLength is not a multiple of 4, any remaining bytes up to the next word boundary are padded with 0.

The length of the destination array must be a multiple of 4, rounded up to the padded sourceLength if required.

Parameters
sourceSource array
destinationDestination array
sourceLengthLength of the source array

§ CryptoUtils_reverseCopy()

void CryptoUtils_reverseCopy ( const void *  source,
void *  destination,
size_t  sourceLength 
)

Reverses and copies an array of bytes.

The source array is reversed byte-wise and copied into the destination array.

Parameters
sourceSource array
destinationDestination array
sourceLengthLength of the source array

§ CryptoUtils_isNumberInRange()

bool CryptoUtils_isNumberInRange ( const void *  number,
size_t  bitLength,
CryptoUtils_Endianess  endianess,
const void *  lowerLimit,
const void *  upperLimit 
)

Checks if number is within the range [lowerLimit, upperLimit)

Checks if the specified number is at greater than or equal to the lower limit and less than the upper limit. Note that the boundary set by the upper limit is not inclusive.

Note that the special values of CryptoUtils_limitZero and CryptoUtils_limitOne are available to pass in for the lowerLimit. (These values can also be used for the upperLimit but their use for the upperLimit has no practical use.)

If lowerLimit is NULL then the lower limit is taken as 0. If upperLimit is NULL then the upper limit is taken as 2(bitLength + 1).

The implemented algorithm is timing-constant when the following parameters are held constant: lowerLimit, upperLimit, bitLength, and endianess. Thus, the number being checked may change and timing will not leak its relation to the limits. However, timing may leak the bitLength, the endianess, and the use of CryptoUtils_limitZero, CryptoUtils_limitOne, and NULL for the limit values.

Parameters
numberPointer to number to check
bitLengthLength in bits of number, lowerLimit, and upperLimit.
endianessThe endianess of number, lowerLimit, and upperLimit.
lowerLimitPointer to lower limit value.
upperLimitPointer to upper limit value.
Return values
trueThe randomNumber is within [lowerLimit, upperLimit).
falseThe randomNumber is not within [lowerLimit, upperLimit).

Variable Documentation

§ CryptoUtils_limitZero

const uint8_t* CryptoUtils_limitZero

Limit value of 0.

This is a value provided for convenience when checking a value against a range.

See also
CryptoUtils_limitOne
CryptoUtils_isNumberInRange

§ CryptoUtils_limitOne

const uint8_t* CryptoUtils_limitOne

Limit value of 1.

This is a value provided for convenience when checking a value against a range.

See also
CryptoUtils_limitZero
CryptoUtils_isNumberInRange
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale