BLE5-Stack 2.01.01 (SDK 3.40) to BLE5-Stack 2.02.01 (SDK 5.10)¶
This section will describe a way to migrate a project from BLE5-Stack 2.01.01 to a BLE5-Stack 2.02.01 project.
The best way to migrate is to open a new project from the new SDK and transfer your changes and application code over to the new example.
Porting Simple Peripheral¶
This section of the migration guide will focus on porting Simple Peripheral from BLE5-Stack 2.01.01 to BLE5-Stack 2.02.01. The recommended approach is to start with a BLE5-Stack 2.02.01 project that contains the same base functionality as the porting target project and merge in any custom functionality.
Choose a BLE5-Stack 2.02.01 example project that contains your target project’s base functionality.
Transfer all modified application files from BLE5-Stack 2.01.01 into the BLE5-Stack 2.02.01 example project.
In this example, the following files from BLE5-Stack 2.01.01 were moved into Simple Peripheral BLE5-Stack 2.02.01 example:
simple_peripheral.c
simple_peripheral.h
Add the pointer
&pRandomAddress
as argument in the last parameter in GAP_DeviceInit call. This is needed to correctly set a random static address if configured.Listing 232. Added section to handle HCI Events for rejection of peer device Connection parameter update request.¶1 GAP_DeviceInit(GAP_PROFILE_PERIPHERAL, selfEntity, addrMode, &pRandomAddress);
Add the following code section in
simple_peripheral.c
at the end of SimplePeripheral_processGapMessage before thedefault:
case:Listing 233. Added section to handle HCI Events for rejection of peer device Connection parameter update request.¶1 #if defined ( NOTIFY_PARAM_UPDATE_RJCT ) 2 case GAP_LINK_PARAM_UPDATE_REJECT_EVENT: 3 { 4 linkDBInfo_t linkInfo; 5 gapLinkUpdateEvent_t *pPkt = (gapLinkUpdateEvent_t *)pMsg; 6 7 // Get the address from the connection handle 8 linkDB_GetInfo(pPkt->connectionHandle, &linkInfo); 9 10 // Display the address of the connection update failure 11 Display_printf(dispHandle, SP_ROW_STATUS_2, 0, 12 "Peer Device's Update Request Rejected 0x%x: %s", pPkt->opcode, 13 Util_convertBdAddr2Str(linkInfo.addr)); 14 15 break; 16 } 17 #endif
Modify
main.c
in the BLE5-Stack 2.02.01 example if additional tasks were added in the BLE5-Stack 2.01.01 project.Move any profiles and services that the application is using to the BLE5-Stack 2.02.01 project.
Transfer the Sysconfig settings either visually through the GUI or open both the old and the new project .syscfg files and copy-paste the desired settings.
If necessary, update the project to use the newer TI-RTOS drivers that are supplied with the SimpleLink CC13xx/CC26xx SDK.
Refer to the Core SDK release notes for additional information and the TI-RTOS examples included with SimpleLink CC13xx/CC26xx SDK.
For additional information on how BLE5-Stack 2.01.02 uses TI-RTOS see TI-RTOS7 (RTOS Kernel) Overview.
For any utilized TI Drivers, review TI-RTOS Kernel (SYS/BIOS) User’s Guide and TI Drivers API Reference.
Porting Simple Central¶
This section of the migration guide will focus on porting Simple Central from BLE5-Stack 2.01.01 to the BLE5-Stack 2.02.01. The recommended approach is to start with a BLE5-Stack 2.02.01 project that contains the same base functionality as theporting target project and merge in any custom functionality.
Choose a BLE5-Stack 2.02.01 example project that contains your target project’s base functionality.
Transfer all modified application files from BLE5-Stack 2.01.01 into the BLE5-Stack 2.02.01 example project.
In this example, the following files from BLE5-Stack 2.01.01 were moved into Simple Central BLE5-Stack 2.02.01 example:
simple_central.c
simple_central.h
Add the pointer
&pRandomAddress
as argument in the last parameter in GAP_DeviceInit call. This is needed to correctly set a random static address if configured.Listing 234. Added section to handle HCI Events for rejection of peer device Connection parameter update request.¶1 GAP_DeviceInit(GAP_PROFILE_CENTRAL, selfEntity, addrMode, &pRandomAddress);
Modify
connRec_t
definition insimple_central.c
such that theaddr
andcharHandle
are of typeuint16_t
as shown below:1 // Connected device information 2 typedef struct 3 { 4 uint16_t connHandle; // Connection Handle 5 uint16_t addr[B_ADDR_LEN]; // Peer Device Address 6 uint16_t charHandle; // Characteristic Handle 7 Clock_Struct *pRssiClock; // pointer to clock struct 8 } connRec_t;
Remove the
DEFAULT_DEV_DISC_BY_SVC_UUID
definition insimple_central.c
as this is now modified through SysConfig.Modify
main.c
in the BLE5-Stack 2.02.01 example if additional tasks were added in the BLE5-Stack 2.01.01 project.Move any profiles and services that the application is using to the BLE5-Stack 2.02.01 project.
Transfer the Sysconfig settings either visually through the GUI or open both the old and the new project .syscfg files and copy-paste the desired settings.
If necessary, update the project to use the newer TI-RTOS drivers that are supplied with the SimpleLink CC13xx/CC26xx SDK.
Refer to the Core SDK release notes for additional information and the TI-RTOS examples included with SimpleLink CC13xx/CC26xx SDK.
For additional information on how BLE5-Stack 2.01.02 uses TI-RTOS see TI-RTOS7 (RTOS Kernel) Overview.
For any utilized TI Drivers, review TI-RTOS Kernel (SYS/BIOS) User’s Guide and TI Drivers API Reference.
RTLS Examples¶
Please refer to the RTLS Toolbox chapter for up-to-date status and information about the RTLS offering. In this section a few application code related changes are listed for your information, but there are more code changes than listed.
Time-of-Flight (TOF) removed from RTLS Toolbox.
Extensive code changes to RTLSCtrl which also includes removal of ToF functionality. Please manually compare files from old and new SDK for more details.
Host Test Example:
Added handling for channel map changes (
HCI_BLE_CHANNEL_MAP_UPDATE_EVENT
).Added compilation options for Constant Tone Extension (
RTLS_CTE_TEST
).
RTLS API
rtls_ctrl_api.h
changesRTLSCtrl_sendDebugEvent
renamed toRTLSCtrl_sendDebugEvt
.RTLSCtrl_processDataSent
renamed toRTLSCtrl_dataSentEvt
.RTLSCtrl_processRtlsPacket
renamed toRTLSCtrl_rtlsPacketEvt
.RTLSCtrl_syncEventNotify
renamed toRTLSCtrl_syncNotifyEvt
.
Updates to rtls_master.c
Added handling for
RM_EVT_CONN_EVT
that will call new functionRTLSMaster_processConnEvt()
.Functionality from
RTLSMaster_connEvtCB
is moved toRTLSMaster_processConnEvt
.Added handling for
HCI_BLE_CHANNEL_MAP_UPDATE_EVENT
.Updated handling for
GAP_LINK_PARAM_UPDATE_EVENT
.Testing of dynamic change of the channel map added (
RTLS_TEST_CHAN_MAP_DYNAMIC_CHANGE
).DEFAULT_MAX_SCAN_RES
changed from 8 to 16.
Updates to rtls_slave
Minor changes to
RTLSPassive_cmStartReq
.AssertHandler added to ubStack_taskFxn.
Small code updates in
micro_ble_cm.c
andmicro_ble_cm.h
Updates to rtls_passive
Only changes related to RTLS API name changes.
Changes in AoA Driver:
AOA_NUM_ANTENNAS
redefined toBOOSTXL_AOA_NUM_ANT
.RF_PriorityCoexDefault
added toAOA_rfEnableRam
.Define
AOA_NUM_ANTENNAS
changed toBOOSTXL_AOA_NUM_ANT
.The
AoA_IQSample_t
struct split into two structs.AoA_IQSample_Ext_t
andAoA_IQSample_t
. This affect code and functions that use it (ex.AOA_getPairAngles
).Changes in
AOA_getPairAngles
parameter.Changes in
AOA_postProcess
parameter.Minor updates in
AOA_getRfIqSamples
.
A Few Noteworthy Changes from BLE5-Stack 2.01.01 to BLE5-Stack 2.02.01¶
You can follow the guide above without addressing these updates, they are listed for your information only. All fine grained details might not be mentioned, please refer to the specific example you need to port and to a compare between the old and new project files. Please refer to the BLE5-Stack Release Notes for all the details.
Handling added in application code for HCI Events for rejection of peer device Connection parameter update request (
NOTIFY_PARAM_UPDATE_RJCT
).Define
NVOCMP_NWSAMEITEM
(set to avoid re-writing the same NV item) and defineFLASH_ROM_BUILD
added to project.Define
DEFAULT_DEV_DISC_BY_SVC_UUID
is now controlled in the checkbox SysConfig->Observer Configuration->Discover Devices By Service UUID. This is used in multi_role and the simple_central example.Privacy Override Offset (
privOverrideOffset
) and CoEx configuration (coexUseCaseConfig
) added tollUserCfg_t
. Configured inble_user_config_stack.c
.Updated code in osal_icall_ble.c to match the extended number of parameters in
GATTServApp_Init()
andGAPBondMgr_Init()
. Parameterscfg_GATTServApp_att_delayed_req
andcfg_GATTServApp_gatt_no_service_changed
are added.GAP Scanner has now the ability to select only to scan on specified channels rather all 3 channels.
Non Volatile On-Chip Multi Page (NVOCMP) Driver now allow the user to check when the next compaction will takes place and receive low voltage detection notifications.
GAPBondMgr can be configured to delete a bond even while the device is in an active connection.
The BLE stack library files (OneLib.a and StackWrapper.a) required by the linker are not directly provided by the .projectspec (CCS) or the .ipcf (IAR). From now on, the file ti_utils_build_linker.cmd.genlibs, generated by SysConfig, includes the libraries required to link the application based on the configurations chosen.
Connectionless-AoA is now supported. For more information, refer to Angle of Arrival.
Periodic Advertisements are now supported. For more information, refer to Periodic Advertising.
TI clang compiler support was added to BLE projects. See Developing a New BLE5-Stack Based Application for a list of projects supported. This change required some modifications to code (i.e. passing in “” to functions that do not receive any input). When porting, no change is required if the legacy compiler is used.
Improvements were made to the BLE5 Stack’s scheduling of events. For details, see Connection Fairness.
A new define was added to gapbondmgr.h.
GAPBOND_AUTHEN_PAIRING_ONLY
is used to enforce authenticated pairing. Additional checks were added to the GAPBondMgr to ensure proper IO capabilities are set when when authenticated pairing is used. Refer to Authentication Pairing Only.The Project Zero data_service.c profile ‘s String Characterisitc Value has been modified to support encrpyted reads/writes. Additionally, in simple_gatt_profile.c, Simple Profile Characteristic 4 Properties were modified to support writes in addition to the original notify support (i.e.
` simpleProfileChar4Props = GATT_PROP_WRITE | GATT_PROP_NOTIFY;)`
)Agama 704 device support has been added to SDK.
Examples for Agama 704 devices have been added to SDK.
Agama 704 devices included in SysConfig.