TI BLE5-Stack API Documentation  2.02.09.00
Data Fields
rtlsSrv_SyncEstEvt_t Struct Reference

Periodic advertising sync establish event structure. More...

Data Fields

uint8_t advAddress [6]
 Advertiser address.
 
uint8_t advAddrType
 Advertiser address type:
0x00 - Public
0x01 - Random
0x02 - Public Identity Address
0x03 - Random Identity Addres.
 
uint8_t advClockAccuracy
 Accuracy of the periodic advertiser's clock:
0x00 - 500 ppm
0x01 - 250 ppm
0x02 - 150 ppm
0x03 - 100 ppm
0x04 - 75 ppm
0x05 - 50 ppm
0x06 - 30 ppm
0x07 - 20 ppm.
 
uint8_t advPhy
 Advertiser PHY:
0x01 - LE 1M
0x02 - LE 2M
0x03 - LE Coded.
 
uint8_t advSid
 Value of the Advertising SID subfield in the ADI field of the PDU.
 
uint8_t opcode
 RTLS event opcode.
 
uint16_t periodicAdvInt
 Periodic advertising interval Range: 0x0006 to 0xFFFF. Time = N * 1.25 ms (Time Range: 7.5 ms to 81.91875 s)
 
uint8_t status
 Periodic advertising sync HCI status.
 
uint16_t syncHandle
 Handle identifying the periodic advertising train.
 

Detailed Description

Periodic advertising sync establish event structure.


The documentation for this struct was generated from the following file:
© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale