TI BLE5-Stack API Documentation  2.02.09.00
Data Fields
hciEvt_BLECteConnectionlessIqReport_t Struct Reference

LE CTE Connectionless IQ Report Event. More...

Data Fields

uint8 BLEEventCode
 BLE Event Code.
 
uint8 channelIndex
 index of channel
 
uint8 cteType
 cte type
 
uint16 eventCounter
 periodic adv event counter
 
osal_event_hdr_t hdr
 osal event header
 
int8 * iqSamples
 list of interleaved I/Q samples
 
uint16 rssi
 current rssi
 
uint8 rssiAntenna
 antenna ID
 
uint8 sampleCount
 number of samples
 
uint8 slotDuration
 sampling slot 1us or 2us
 
uint8 status
 packet status (success or CRC error)
 
uint16 syncHandle
 sync handle in periodic adv
 

Detailed Description

LE CTE Connectionless IQ Report Event.


The documentation for this struct was generated from the following file:
© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale