TI BLE5-Stack API Documentation  2.02.09.00
Data Fields
gapBondRec_t Struct Reference

Structure of NV data for the connected device's address information. More...

Data Fields

uint8_t addr [B_ADDR_LEN]
 
GAP_Peer_Addr_Types_t addrType
 
uint8_t stateFlags
 

Detailed Description

Structure of NV data for the connected device's address information.

Field Documentation

§ addr

uint8_t addr[B_ADDR_LEN]

Peer's address

If identity information exists for this bond, this will be an identity address

§ addrType

Peer's address type

§ stateFlags

uint8_t stateFlags

State flags of bond

GAP_BONDED_STATE_FLAGS


The documentation for this struct was generated from the following file:
© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale