![]() |
![]() |
SYS/BIOS
7.00
|
Heap manager that enables tracking of all allocated blocks.
HeapTrack manager provides functions to allocate and free storage from a configured heap which inherits from IHeap. The calling context is going to match the heap being used.
HeapTrack is useful for detecting memory leaks, double frees and buffer overflows. There is a performance overhead cost when using heap track as well as a size impact. Every alloc will include a HeapTrack_Tracker structure (plus memory to get proper alignment of the stucture) at the end of the buffer that should not be modified by the user. It is important to remember this when deciding on heap sizes and you may have to adjust the total size or buffer sizes (for HeapBuf/HeapMultiBuf).
ROV displays peaks and current in-use for both allocated memory (requested size + Tracker structure) and requested memory (without Tracker).
The information stored in the tracker packet is used to display information in RTOS Object Viewer (ROV) as well as with the printTask and printHeap functions.
The asserts used in this module are listed below and include error checking for double frees, calling printHeap with a null handle, buffer overflows and deleting a non empty heap.
#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
#include <ti/sysbios/knl/Queue.h>
#include <ti/sysbios/knl/Task.h>
#include <ti/sysbios/runtime/Error.h>
#include <ti/sysbios/runtime/IHeap.h>
#include <ti/sysbios/runtime/Memory.h>
Go to the source code of this file.
Data Structures | |
struct | HeapTrack_Tracker |
Structure added to the end of each allocated block. More... | |
struct | HeapTrack_Params |
struct | HeapTrack_Struct |
struct | HeapTrack_Module_State |
Macros | |
#define | HeapTrack_A_doubleFree "Buffer already free" |
Assert raised when freeing a buffer that was already freed. More... | |
#define | HeapTrack_A_bufOverflow "Buffer overflow" |
Assert raised when freeing memory with corrupted data or using the wrong size. More... | |
#define | HeapTrack_A_notEmpty "Heap not empty" |
Assert raised when deleting a non-empty heap. More... | |
#define | HeapTrack_A_nullObject "HeapTrack_printHeap called with null obj" |
Assert raised when calling printTask with a null HeapTrack object. More... | |
#define | ti_sysbios_heaps_HeapTrack_Handle_upCast(handle) ((IHeap_Handle)(handle)) |
cast handle to an IHeap_Handle for use by Memory_alloc, etc. More... | |
Typedefs | |
typedef struct HeapTrack_Struct * | HeapTrack_Handle |
typedef HeapTrack_Struct | HeapTrack_Object |
Functions | |
void * | HeapTrack_alloc (HeapTrack_Handle heap, size_t size, size_t align, Error_Block *eb) |
Allocate a block of memory from the heap. More... | |
void | HeapTrack_free (HeapTrack_Handle heap, void *buf, size_t size) |
Free a block of memory back to the heap. More... | |
bool | HeapTrack_isBlocking (HeapTrack_Handle heap) |
Can this heap block the caller. More... | |
void | HeapTrack_getStats (HeapTrack_Handle heap, Memory_Stats *stats) |
get memory stats for a HeapTrack object More... | |
void | HeapTrack_printTask (Task_Handle task) |
Print out the blocks that are currently allocated by a task. More... | |
void | HeapTrack_printHeap (HeapTrack_Handle heap) |
Print details for a HeapTrack instance. More... | |
HeapTrack_Handle | HeapTrack_Object_first (void) |
return handle of the first HeapTrack on HeapTrack list More... | |
HeapTrack_Handle | HeapTrack_Object_next (HeapTrack_Handle heap) |
return handle of the next HeapTrack on HeapTrack list More... | |
HeapTrack_Handle | HeapTrack_create (const HeapTrack_Params *params, Error_Block *eb) |
Create a HeapTrack heap. More... | |
HeapTrack_Handle | HeapTrack_construct (HeapTrack_Struct *obj, const HeapTrack_Params *params) |
Construct a HeapTrack heap. More... | |
void | HeapTrack_delete (HeapTrack_Handle *heap) |
Delete a HeapTrack heap. More... | |
void | HeapTrack_destruct (HeapTrack_Struct *obj) |
Destruct a HeapTrack heap. More... | |
void | HeapTrack_Params_init (HeapTrack_Params *prms) |
Initialize the HeapTrack_Params structure with default values. More... | |
static HeapTrack_Handle | HeapTrack_handle (HeapTrack_Struct *str) |
static HeapTrack_Struct * | HeapTrack_struct (HeapTrack_Handle h) |
#define HeapTrack_A_doubleFree "Buffer already free" |
Assert raised when freeing a buffer that was already freed.
#define HeapTrack_A_bufOverflow "Buffer overflow" |
Assert raised when freeing memory with corrupted data or using the wrong size.
#define HeapTrack_A_notEmpty "Heap not empty" |
Assert raised when deleting a non-empty heap.
#define HeapTrack_A_nullObject "HeapTrack_printHeap called with null obj" |
Assert raised when calling printTask with a null HeapTrack object.
#define ti_sysbios_heaps_HeapTrack_Handle_upCast | ( | handle | ) | ((IHeap_Handle)(handle)) |
cast handle to an IHeap_Handle for use by Memory_alloc, etc.
handle | heap handle |
IHeap_Handle |
typedef struct HeapTrack_Struct * HeapTrack_Handle |
typedef HeapTrack_Struct HeapTrack_Object |
void* HeapTrack_alloc | ( | HeapTrack_Handle | heap, |
size_t | size, | ||
size_t | align, | ||
Error_Block * | eb | ||
) |
Allocate a block of memory from the heap.
void HeapTrack_free | ( | HeapTrack_Handle | heap, |
void * | buf, | ||
size_t | size | ||
) |
Free a block of memory back to the heap.
bool HeapTrack_isBlocking | ( | HeapTrack_Handle | heap | ) |
Can this heap block the caller.
HeapTrack
returns true
if the underlying heap is blocking. HeapTrack
returns false
if the underlying heap not blocking.
heap | heap handle |
<tt>true</tt> | if the underlying heap if blocking, false otherwise |
void HeapTrack_getStats | ( | HeapTrack_Handle | heap, |
Memory_Stats * | stats | ||
) |
get memory stats for a HeapTrack object
heap | heap handle |
stats | pointer to a Memory_Stats object |
void HeapTrack_printTask | ( | Task_Handle | task | ) |
Print out the blocks that are currently allocated by a task.
Iterates through all instances of HeapTrack and prints out information about all allocated blocks of memory for a given task handle. This function is not thread safe.
void HeapTrack_printHeap | ( | HeapTrack_Handle | heap | ) |
Print details for a HeapTrack instance.
Print the details of all allocated blocks of memory for a HeapTrack instance. This function is not thread safe.
HeapTrack_Handle HeapTrack_Object_first | ( | void | ) |
return handle of the first HeapTrack on HeapTrack list
Return the handle of the first HeapTrack on the create/construct list. NULL if no HeapTracks have been created or constructed.
HeapTrack | handle |
HeapTrack_Handle HeapTrack_Object_next | ( | HeapTrack_Handle | heap | ) |
return handle of the next HeapTrack on HeapTrack list
Return the handle of the next HeapTrack on the create/construct list. NULL if no more HeapTracks are on the list.
heap | HeapTrack handle |
HeapTrack | handle |
HeapTrack_Handle HeapTrack_create | ( | const HeapTrack_Params * | params, |
Error_Block * | eb | ||
) |
Create a HeapTrack
heap.
params | optional parameters |
eb | error block |
HeapTrack | handle (NULL on failure) |
HeapTrack_Handle HeapTrack_construct | ( | HeapTrack_Struct * | obj, |
const HeapTrack_Params * | params | ||
) |
Construct a HeapTrack
heap.
HeapTrack_construct is equivalent to HeapTrack_create except that the HeapTrack_Struct is pre-allocated.
obj | pointer to a HeapTrack object |
params | optional parameters |
HeapTrack | handle (NULL on failure) |
void HeapTrack_delete | ( | HeapTrack_Handle * | heap | ) |
Delete a HeapTrack
heap.
Note that HeapTrack_delete takes a pointer to a HeapTrack_Handle which enables HeapTrack_delete to set the HeapTrack handle to NULL.
heap | pointer to a HeapTrack handle |
void HeapTrack_destruct | ( | HeapTrack_Struct * | obj | ) |
Destruct a HeapTrack
heap.
obj | pointer to a HeapTrack objects |
void HeapTrack_Params_init | ( | HeapTrack_Params * | prms | ) |
Initialize the HeapTrack_Params structure with default values.
HeapTrack_Params_init initializes the HeapTrack_Params structure with default values. HeapTrack_Params_init should always be called before setting individual parameter fields. This allows new fields to be added in the future with compatible defaults – existing source code does not need to change when new fields are added.
prms | pointer to uninitialized params structure |
|
inlinestatic |
|
inlinestatic |