SYS/BIOS
7.00
|
Data Fields | |
uintptr_t | arg |
User supplied argument for the user supplied create function. More... | |
uintptr_t HeapCallback_Params::arg |
User supplied argument for the user supplied create function.
This user supplied argument will be passed back as an argument to the createInstFxn
function. It can be used by the createInstFxn function at runtime to differentiate between the multiple Heap instances configured in the user config script.
The user can skip configuring this argument. In such a case, the default value 0
will be passed back as an argument to the createInstFxn
function.