Radio Software Bundle (rflib) 7.10.03.08 Release Notes
Table of Contents
Introduction
The Radio Software Bundle (RFLib) component for CC13xx and CC26xx consists of:
- The high-level RF driver
- SysConfig meta data for configuring the RF driver and the front-end
- SysConfig meta data for configuring radio PHYs
- Low-level radio access functions used by the RF driver
- RF Core firmware patches for various PHYs
- API documentation
Documentation
The following documentation is included in RFLib.
- RFLib Software Manifest
- API documentation
- Release Notes (this document)
Disclaimer
CC1312PSIP: Regulation of TX power vs VDDS (3.3V-3.8V)
TX power is regulated for power supply voltage changes in the CC1312PSIP device. This reduces the effect of increasing VDDS on the TX power and limits the TX power from going much higher than 20 dBm. The TX power regulation is applied when VDDS > 3.3V and the device is set to transmit 17 dBm or above.
Under these conditions, the feature maintains the TX power close to the original power setting even when VDDS is increased. For TX power setting below 17 dBm, the feature has no effect on the device behavior.
RF Sysconfig: Antenna Switch Hardware Changes
The antenna switch, available under “Use Hardware”, is required by P device boards (matching regex /CC....P/). To ensure correct RF performance, the correct value for this option is now selected by default in the UI, but not when adding the RF module in a config script.
Make sure this option is selected for correct RF performance. It must also be placed before any assignments related to the RF module for coex.
See snippet below to add correct hardware:
const RF = scripting.addModule("/ti/drivers/RF");
if (("board" in system.deviceData) && ("RF" in system.deviceData.board.components)) {
RF.$hardware = system.deviceData.board.components.RF;
}What’s New
| ID | Summary |
|---|---|
| RFDRIVER-470 | CC13x4: Add support for increased Sub-1GHz PA table resolution |
| RFDRIVER-782 | Change RF driver SWTCXO command termination from abort to graceful stop |
| RFCORE-961 | CC2652R-Q1: PA Table Update - Improved Performance |
| RFCORE-1009 | CC1312PSIP: PA Table Update - New High PA Entries |
| RFCORE-987 | cc13x4_cc26x4: Settings Release - 5/20 dBm: WB-DSSS - Release Candidate |
| RFCORE-932 | CC1312PSIP: Settings Release - 14 dBm: 50 kbps/ 200 kbps / 1 Mbps 2-GFSK - Characterized |
| RFCORE-967 | cc13x4_cc26x4: Settings Release - 20 dBm: PROP 16.384 kbps OOK, Manchester encoding - Characterized |
| RFCORE-971 | cc13x4_cc26x4: Settings Release - 5/20 dBm: BLE 1M, 2M, Coded and IEEE 802.15.4 (ZigBee) - Characterized |
| RFCORE-980 | CC1314R, CC1354P/R: PA Table Update - Increased Sub-1GHz Granularity |
| RFCORE-972 | cc13x4_cc26x4: PA Table Update - Increased Sub-1GHz Granularity |
| RFCORE-1016 | cc13x4_cc26x4: Settings Release - 20dBm: IEEE 802.15.4 (ZigBee) - Characterized |
| RFCORE-993 | cc13x4: Settings Release - 5/20dBm: Sub1GHz WB-DSSS, 50Kbps - Characterized |
| RFCORE-924 | cc13x4_cc26x4: Settings Release - 5 dBm: 50/25/12.5/6.25 kbps SUN O-QPSK - Release Candidate |
| RFCORE-982 | CC2674R10: Settings Release - 5 dBm: ZigBee Frontend ID - Characterized |
| RFCORE-892 | cc13x1_cc26x1: Settings Update - Patch: Remove deprecated “rf_patch_cpe_multi_protocol” |
| RFCORE-966 | CC1312PSIP: PA Table Update - 20 dBm: Characterized |
| RFCORE-965 | CC1312PSIP: Settings Release - 20 dBm: 50 kbps 2-GFSK - Characterized |
| RFCORE-964 | CC1312PSIP: Settings Release - 20 dBm: Zigbee R23 500 kbps 2-GFSK - Characterized |
| RFCORE-933 | CC1312PSIP: PA Table Update - 14 dBm: Characterized |
| RFCORE-934 | CC1312PSIP: Settings Release - 14 dBm: Wireless MBUS S1-/S2-/T-/C-Mode - Characterized |
| RFCORE-931 | CC1312PSIP: Settings Release - 14 dBm: 9.6 kbps Narrowband - Characterized |
| RFCORE-927 | cc13x4_cc26x4: Settings Release - 5/14 dBm: PROP 16.384 kbps OOK, Manchester encoding - Characterized |
| RFCORE-944 | CC1312PSIP: Settings Release - 14 dBm: Wi-SUN Mode #1-5 - Characterized |
| RFCORE-952 | CC1312PSIP: Settings Release - 14 dBm: 4.8 kbps OOK - Characterized |
| RFCORE-940 | CC1312PSIP: Settings Release - 14 dBm: SimpleLink Long Range 2.5/5 kbps - Characterized |
| RFCORE-938 | CC1312PSIP: Settings Release - 14 dBm: Zigbee R23 100/500 kbps 2-GFSK - Characterized |
| RFCORE-953 | CC1312PSIP: Settings Release - 14 dBm: WB-DSSS 240/120/60/30 kbps with 1/2/4/8 x spreading - Characterized |
| RFCORE-979 | CC1311R: PA Table Update - New entries for 868/915 MHz PHYs |
Fixed Issues
| ID | Summary |
|---|---|
| RFDRIVER-743 | cc13x2_cc26x2: SysConfig generates incorrect pOverrides_ble2Mbps when enabling BLE 2M PHY and Coexistence |
| RFCORE-983 | cc13x4_cc26x4: Incorrect interrupt priorities cause IEEE CSMA command to stall indefinitely |
Known Issues
| ID | Summary |
|---|---|
| None | None |
Upgrade and Compatibility Information
This release breaks compatibility with previous releases of RFLib in the following ways:
cc13x1_cc26x1: The CPE multi protocol patch (rf_patch_cpe_multi_protocol) is deprecated and removed.- Any generated settings previously using this patch are updated to refer to the specific protocol patches
rf_patch_cpe[bt5, ieee_802_15_4, prop].
Versioning
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.