rflib
Data Fields
rfc_CMD_PROP_TX_ADV_s Struct Reference

Proprietary Mode Advanced Transmit Command. More...

#include <rf_prop_cmd.h>

Collaboration diagram for rfc_CMD_PROP_TX_ADV_s:
Collaboration graph
[legend]

Data Fields

uint16_t commandNo
 The command ID number 0x3803. More...
 
uint16_t status
 An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More...
 
rfc_radioOp_tpNextOp
 Pointer to the next operation to run after this operation is done. More...
 
ratmr_t startTime
 Absolute or relative start time (depending on the value of startTrigger) More...
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
startTrigger
 Identification of the trigger that starts the operation. More...
 
struct {
   uint8_t   rule:4
 Condition for running next command: Rule for how to proceed. More...
 
   uint8_t   nSkip:4
 Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More...
 
condition
 
struct {
   uint8_t   bFsOff:1
 0: Keep frequency synth on after command
1: Turn frequency synth off after command More...
 
   uint8_t   __pad0__:2
 
   uint8_t   bUseCrc:1
 0: Do not append CRC
1: Append CRC More...
 
   uint8_t   bCrcIncSw:1
 0:Do not include sync word in CRC calculation
1: Include sync word in CRC calculation More...
 
   uint8_t   bCrcIncHdr:1
 0: Do not include header in CRC calculation
1: Include header in CRC calculation More...
 
pktConf
 
uint8_t numHdrBits
 Number of bits in header (0–32) More...
 
uint16_t pktLen
 Packet length. 0: Unlimited. More...
 
struct {
   uint8_t   bExtTxTrig:1
 0: Start packet on a fixed time from the command start trigger
1: Start packet on an external trigger (input event to RAT) More...
 
   uint8_t   inputMode:2
 Input mode if external trigger is used for TX start
0: Rising edge
1: Falling edge
2: Both edges
3: Reserved More...
 
   uint8_t   source:5
 RAT input event number used for capture if external trigger is used for TX start. More...
 
startConf
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
preTrigger
 Trigger for transition from preamble to sync word. More...
 
ratmr_t preTime
 Time used together with preTrigger for transition from preamble to sync word. If preTrigger.triggerType is set to "now", one preamble as configured in the setup will be sent. Otherwise, the preamble will be repeated until this trigger is observed. More...
 
uint32_t syncWord
 Sync word to transmit. More...
 
uint8_t * pPkt
 Pointer to packet, or TX queue for unlimited length. More...
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
startTrigger
 Identification of the trigger that starts the operation. More...
 
struct {
   uint8_t   rule:4
 Condition for running next command: Rule for how to proceed. More...
 
   uint8_t   nSkip:4
 Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More...
 
condition
 
struct {
   uint8_t   bFsOff:1
 0: Keep frequency synth on after command
1: Turn frequency synth off after command More...
 
   uint8_t   __pad0__:2
 
   uint8_t   bUseCrc:1
 0: Do not append CRC
1: Append CRC More...
 
   uint8_t   bCrcIncSw:1
 0:Do not include sync word in CRC calculation
1: Include sync word in CRC calculation More...
 
   uint8_t   bCrcIncHdr:1
 0: Do not include header in CRC calculation
1: Include header in CRC calculation More...
 
pktConf
 
struct {
   uint8_t   bExtTxTrig:1
 0: Start packet on a fixed time from the command start trigger
1: Start packet on an external trigger (input event to RAT) More...
 
   uint8_t   inputMode:2
 Input mode if external trigger is used for TX start
0: Rising edge
1: Falling edge
2: Both edges
3: Reserved More...
 
   uint8_t   source:5
 RAT input event number used for capture if external trigger is used for TX start. More...
 
startConf
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
preTrigger
 Trigger for transition from preamble to sync word. More...
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
startTrigger
 Identification of the trigger that starts the operation. More...
 
struct {
   uint8_t   rule:4
 Condition for running next command: Rule for how to proceed. More...
 
   uint8_t   nSkip:4
 Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More...
 
condition
 
struct {
   uint8_t   bFsOff:1
 0: Keep frequency synth on after command
1: Turn frequency synth off after command More...
 
   uint8_t   __pad0__:2
 
   uint8_t   bUseCrc:1
 0: Do not append CRC
1: Append CRC More...
 
   uint8_t   bCrcIncSw:1
 0:Do not include sync word in CRC calculation
1: Include sync word in CRC calculation More...
 
   uint8_t   bCrcIncHdr:1
 0: Do not include header in CRC calculation
1: Include header in CRC calculation More...
 
pktConf
 
struct {
   uint8_t   bExtTxTrig:1
 0: Start packet on a fixed time from the command start trigger
1: Start packet on an external trigger (input event to RAT) More...
 
   uint8_t   inputMode:2
 Input mode if external trigger is used for TX start
0: Rising edge
1: Falling edge
2: Both edges
3: Reserved More...
 
   uint8_t   source:5
 RAT input event number used for capture if external trigger is used for TX start. More...
 
startConf
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
preTrigger
 Trigger for transition from preamble to sync word. More...
 

Detailed Description

Proprietary Mode Advanced Transmit Command.

Field Documentation

§ commandNo

uint16_t rfc_CMD_PROP_TX_ADV_s::commandNo

The command ID number 0x3803.

§ status

uint16_t rfc_CMD_PROP_TX_ADV_s::status

An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.

§ pNextOp

rfc_radioOp_t * rfc_CMD_PROP_TX_ADV_s::pNextOp

Pointer to the next operation to run after this operation is done.

§ startTime

ratmr_t rfc_CMD_PROP_TX_ADV_s::startTime

Absolute or relative start time (depending on the value of startTrigger)

§ triggerType

uint8_t rfc_CMD_PROP_TX_ADV_s::triggerType

The type of trigger.

§ bEnaCmd

uint8_t rfc_CMD_PROP_TX_ADV_s::bEnaCmd

0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger

§ triggerNo

uint8_t rfc_CMD_PROP_TX_ADV_s::triggerNo

The trigger number of the CMD_TRIGGER command that triggers this action.

§ pastTrig

uint8_t rfc_CMD_PROP_TX_ADV_s::pastTrig

0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible

§ startTrigger [1/3]

struct { ... } rfc_CMD_PROP_TX_ADV_s::startTrigger

Identification of the trigger that starts the operation.

§ rule

uint8_t rfc_CMD_PROP_TX_ADV_s::rule

Condition for running next command: Rule for how to proceed.

§ nSkip

uint8_t rfc_CMD_PROP_TX_ADV_s::nSkip

Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ...

§ condition [1/3]

struct { ... } rfc_CMD_PROP_TX_ADV_s::condition

§ bFsOff

uint8_t rfc_CMD_PROP_TX_ADV_s::bFsOff

0: Keep frequency synth on after command
1: Turn frequency synth off after command

§ __pad0__

uint8_t rfc_CMD_PROP_TX_ADV_s::__pad0__

§ bUseCrc

uint8_t rfc_CMD_PROP_TX_ADV_s::bUseCrc

0: Do not append CRC
1: Append CRC

§ bCrcIncSw

uint8_t rfc_CMD_PROP_TX_ADV_s::bCrcIncSw

0:Do not include sync word in CRC calculation
1: Include sync word in CRC calculation

§ bCrcIncHdr

uint8_t rfc_CMD_PROP_TX_ADV_s::bCrcIncHdr

0: Do not include header in CRC calculation
1: Include header in CRC calculation

§ pktConf [1/3]

struct { ... } rfc_CMD_PROP_TX_ADV_s::pktConf

§ numHdrBits

uint8_t rfc_CMD_PROP_TX_ADV_s::numHdrBits

Number of bits in header (0–32)

§ pktLen

uint16_t rfc_CMD_PROP_TX_ADV_s::pktLen

Packet length. 0: Unlimited.

§ bExtTxTrig

uint8_t rfc_CMD_PROP_TX_ADV_s::bExtTxTrig

0: Start packet on a fixed time from the command start trigger
1: Start packet on an external trigger (input event to RAT)

§ inputMode

uint8_t rfc_CMD_PROP_TX_ADV_s::inputMode

Input mode if external trigger is used for TX start
0: Rising edge
1: Falling edge
2: Both edges
3: Reserved

§ source

uint8_t rfc_CMD_PROP_TX_ADV_s::source

RAT input event number used for capture if external trigger is used for TX start.

§ startConf [1/3]

struct { ... } rfc_CMD_PROP_TX_ADV_s::startConf

§ preTrigger [1/3]

struct { ... } rfc_CMD_PROP_TX_ADV_s::preTrigger

Trigger for transition from preamble to sync word.

§ preTime

ratmr_t rfc_CMD_PROP_TX_ADV_s::preTime

Time used together with preTrigger for transition from preamble to sync word. If preTrigger.triggerType is set to "now", one preamble as configured in the setup will be sent. Otherwise, the preamble will be repeated until this trigger is observed.

§ syncWord

uint32_t rfc_CMD_PROP_TX_ADV_s::syncWord

Sync word to transmit.

§ pPkt

uint8_t * rfc_CMD_PROP_TX_ADV_s::pPkt

Pointer to packet, or TX queue for unlimited length.

§ startTrigger [2/3]

struct { ... } rfc_CMD_PROP_TX_ADV_s::startTrigger

Identification of the trigger that starts the operation.

§ condition [2/3]

struct { ... } rfc_CMD_PROP_TX_ADV_s::condition

§ pktConf [2/3]

struct { ... } rfc_CMD_PROP_TX_ADV_s::pktConf

§ startConf [2/3]

struct { ... } rfc_CMD_PROP_TX_ADV_s::startConf

§ preTrigger [2/3]

struct { ... } rfc_CMD_PROP_TX_ADV_s::preTrigger

Trigger for transition from preamble to sync word.

§ startTrigger [3/3]

struct { ... } rfc_CMD_PROP_TX_ADV_s::startTrigger

Identification of the trigger that starts the operation.

§ condition [3/3]

struct { ... } rfc_CMD_PROP_TX_ADV_s::condition

§ pktConf [3/3]

struct { ... } rfc_CMD_PROP_TX_ADV_s::pktConf

§ startConf [3/3]

struct { ... } rfc_CMD_PROP_TX_ADV_s::startConf

§ preTrigger [3/3]

struct { ... } rfc_CMD_PROP_TX_ADV_s::preTrigger

Trigger for transition from preamble to sync word.


The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale