Data Fields
TRNG_s_RandomBytesSecureCallback Struct Reference

#include <TRNGCC26X4_s.h>

Collaboration diagram for TRNG_s_RandomBytesSecureCallback:
Collaboration graph
[legend]

Data Fields

SecureCallback_Object object
 
TRNG_Handle handle
 
int_fast16_t returnValue
 
uint8_t * randomBytes
 
size_t randomBytesSize
 

Field Documentation

§ object

SecureCallback_Object TRNG_s_RandomBytesSecureCallback::object

§ handle

TRNG_Handle TRNG_s_RandomBytesSecureCallback::handle

§ returnValue

int_fast16_t TRNG_s_RandomBytesSecureCallback::returnValue

§ randomBytes

uint8_t* TRNG_s_RandomBytesSecureCallback::randomBytes

§ randomBytesSize

size_t TRNG_s_RandomBytesSecureCallback::randomBytesSize

The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale