Data Fields
FlashCC26X4_s_program Struct Reference

#include <FlashCC26X4_s.h>

Data Fields

uint8_t * dataBuffer
 
uint32_t sectorAddress
 
uint32_t count
 

Field Documentation

§ dataBuffer

uint8_t* FlashCC26X4_s_program::dataBuffer

§ sectorAddress

uint32_t FlashCC26X4_s_program::sectorAddress

§ count

uint32_t FlashCC26X4_s_program::count

The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale