CUI API  1.00.00.00
Data Fields
CUI_clientParams_t Struct Reference

#include <cui.h>

Data Fields

char clientName [MAX_CLIENT_NAME_LEN]
 
uint8_t maxStatusLines
 

Field Documentation

§ clientName

char CUI_clientParams_t::clientName[MAX_CLIENT_NAME_LEN]

§ maxStatusLines

uint8_t CUI_clientParams_t::maxStatusLines

The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale