![]() |
![]() |
TI BLE5-Stack API Documentation
2.02.08.01
|
Params used in the GapAdv module
enum GapAdv_ParamId_t |
GAP Advertising Parameters
These can be set with GapAdv_setParam and read with GapAdv_getParam. They do not have default values since it is required to pass a set of parameters into GapAdv_create
Each advertising handle can have a different set of parameters.
All parameters are readable and writable
Enumerator | |
---|---|
GAP_ADV_PARAM_PROPS | Advertising Event Properties size: uint16_t range: GapAdv_eventProps_t |
GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN | Minimum advertising interval (n * 0.625 ms) This is for undirected and low duty cycle directed advertising size: uint32_t range: 20 ms to 10,485.759375 s |
GAP_ADV_PARAM_PRIMARY_INTERVAL_MAX | Maximum advertising interval (n * 0.625 ms This is for undirected and low duty cycle directed advertising
size: uint32_t range: 20 ms to 10,485.759375 s |
GAP_ADV_PARAM_PRIMARY_CHANNEL_MAP | Primary Channel Map A bit field that indicates the advertising channels that shall be used when transmitting advertising packets size: uint8_t range: GapAdv_advChannels_t |
GAP_ADV_PARAM_PEER_ADDRESS_TYPE | Peer Address Type for Directed Advertising size: uint8_t range: GAP_Peer_Addr_Types_t |
GAP_ADV_PARAM_PEER_ADDRESS | Peer Address for Directed Advertising size: uint8_t[6] range: 0x000000000000 - 0xFFFFFFFFFFFE |
GAP_ADV_PARAM_FILTER_POLICY | Advertising Filter Policy size: uint8_t range: GapAdv_filterPolicy_t |
GAP_ADV_PARAM_TX_POWER | Advertising Tx Power This is the maximum power level at which the advertising packets are to be transmitted on the advertising channels. The Controller will choose a power level lower than or equal to this.
size: int8_t units: dBm range: -127 to +20 or GAP_ADV_TX_POWER_NO_PREFERENCE |
GAP_ADV_PARAM_PRIMARY_PHY | Primary PHY The PHY on which the advertising packets are transmitted on the primary advertising channel. size: uint8_t range: GapAdv_primaryPHY_t |
GAP_ADV_PARAM_SECONDARY_PHY | Secondary PHY The PHY on which the advertising packets are be transmitted on the secondary advertising channel. size: uint8_t range: GapAdv_secondaryPHY_t |
GAP_ADV_PARAM_SID | Advertising SID (set identity) This is the value to be transmitted in the Advertising SID subfield of the ADI field of the Extended Header of those advertising channel PDUs that have an ADI field. If the advertising set only uses PDUs that do not contain an ADI field, this parameter is ignored. size: uint8_t range: 0-15 |
GAP_ADV_PARAM_OWN_ADDRESS_TYPE | Own address type of the advSet This is the value of the address type that can determine of which address the device will advertise with. The value can be set only if the gapDeviceAddrMode is set to RPA. 0x00 - Public address (IDA). 0x01 - Random address (Static Random). 0x02 - RPA with public. 0x03 - RPA with random. size: uint8_t range: 0x00-0x03 |