![]() |
![]() |
TI BLE5-Stack API Documentation
2.02.08.01
|
Macros | |
#define | GAPBOND_GENERATE_ECC_DONE 0x06 |
Get ECC keys done. | |
#define | GAPBOND_PAIRING_STATE_BOND_SAVED 0x03 |
Bonding record saved in NV. | |
#define | GAPBOND_PAIRING_STATE_CAR_READ 0x04 |
Central Address Resolution Characteristic Read. | |
#define | GAPBOND_PAIRING_STATE_COMPLETE 0x01 |
#define | GAPBOND_PAIRING_STATE_ENCRYPTED 0x02 |
#define | GAPBOND_PAIRING_STATE_RPAO_READ 0x05 |
Resolvable Private Address Only Characteristic Read. | |
#define | GAPBOND_PAIRING_STATE_STARTED 0x00 |
These are the states that are returned through the pfnPairStateCB_t. See the specific state for its possible statuses.
#define GAPBOND_PAIRING_STATE_COMPLETE 0x01 |
Pairing Complete
The following statuses are possible for this state: SUCCESS : pairing pairing is complete (Session keys have been exchanged) SMP_PAIRING_FAILED_PASSKEY_ENTRY_FAILED : user input failed SMP_PAIRING_FAILED_OOB_NOT_AVAIL : Out-of-band data not available SMP_PAIRING_FAILED_AUTH_REQ : Input and output capabilities of devices do not allow for authentication SMP_PAIRING_FAILED_CONFIRM_VALUE : the confirm value does not match the calculated compare value SMP_PAIRING_FAILED_NOT_SUPPORTED : pairing is unsupported SMP_PAIRING_FAILED_ENC_KEY_SIZE : encryption key size is insufficient SMP_PAIRING_FAILED_CMD_NOT_SUPPORTED : The SMP command received is unsupported on this device SMP_PAIRING_FAILED_UNSPECIFIED : encryption failed to start bleTimeout : pairing failed to complete before timeout bleGAPBondRejected : keys did not match
#define GAPBOND_PAIRING_STATE_ENCRYPTED 0x02 |
Encryption has started
This event is returned after encryption has started, either using the keys from the pairing that has just completed, or using keys from NV for a bonded device.
The following statuses are possible for this state: SUCCESS : pairing has been initiated. A pairing request has been either sent or received. HCI_ERROR_CODE_PIN_KEY_MISSING : encryption key is missing HCI_ERROR_CODE_UNSUPPORTED_REMOTE_FEATURE : feature is unsupported by the remote device HCI_ERROR_CODE_LMP_LL_RESP_TIMEOUT : Timeout waiting for response bleGAPBondRejected (0x32): this is received due to one of the previous three errors
#define GAPBOND_PAIRING_STATE_STARTED 0x00 |
Pairing Started
The following statuses are possible for this state: SUCCESS : pairing has been initiated. A pairing request has been either sent or received.