TI BLE5-Stack API Documentation  2.02.08.01
gap_advertiser.h
Go to the documentation of this file.
1 /******************************************************************************
2 
3  Group: WCS, BTS
4  $Target Device: DEVICES $
5 
6  ******************************************************************************
7  $License: TI_TEXT 2009 $
8  ******************************************************************************
9  $Release Name: PACKAGE NAME $
10  $Release Date: PACKAGE RELEASE DATE $
11  *****************************************************************************/
12 
22 #ifndef GAP_ADVERTISER_H
23 #define GAP_ADVERTISER_H
24 
25 #ifdef __cplusplus
26 extern "C"
27 {
28 #endif
29 
30 /*-------------------------------------------------------------------
31  * INCLUDES
32  */
33 #include "bcomdef.h"
34 #include "osal.h"
35 #include "gap.h"
36 
37 /*-------------------------------------------------------------------
38  * MACROS
39  */
40 
41 // This is a common file for the legacy and sysconfig examples,
42 // the parameters under ifndef SYSCFG are defined in this file for
43 // the legacy examples and generated using the sysconfig tool for
44 // the sysconfig examples
45 #ifndef SYSCFG
46 
52 #define GAPADV_PARAMS_LEGACY_SCANN_CONN { \
54  .eventProps = GAP_ADV_PROP_CONNECTABLE | GAP_ADV_PROP_SCANNABLE | \
55  GAP_ADV_PROP_LEGACY, \
56  .primIntMin = 160, \
57  .primIntMax = 160, \
58  .primChanMap = GAP_ADV_CHAN_ALL, \
59  .peerAddrType = PEER_ADDRTYPE_PUBLIC_OR_PUBLIC_ID, \
60  .peerAddr = { 0xaa, 0xaa, 0xaa, 0xaa, 0xaa, 0xaa }, \
61  .filterPolicy = GAP_ADV_WL_POLICY_ANY_REQ, \
62  .txPower = GAP_ADV_TX_POWER_NO_PREFERENCE, \
63  .primPhy = GAP_ADV_PRIM_PHY_1_MBPS, \
64  .secPhy = GAP_ADV_SEC_PHY_1_MBPS, \
65  .sid = 0 \
66 }
67 
69 #define GAPADV_PARAMS_AE_LONG_RANGE_CONN { \
70  .eventProps = GAP_ADV_PROP_CONNECTABLE, \
71  .primIntMin = 160, \
72  .primIntMax = 160, \
73  .primChanMap = GAP_ADV_CHAN_ALL, \
74  .peerAddrType = PEER_ADDRTYPE_PUBLIC_OR_PUBLIC_ID, \
75  .peerAddr = { 0xaa, 0xaa, 0xaa, 0xaa, 0xaa, 0xaa }, \
76  .filterPolicy = GAP_ADV_WL_POLICY_ANY_REQ, \
77  .txPower = GAP_ADV_TX_POWER_NO_PREFERENCE, \
78  .primPhy = GAP_ADV_PRIM_PHY_CODED_S2, \
79  .secPhy = GAP_ADV_SEC_PHY_CODED_S2, \
80  .sid = 0 \
81 }
82 
84 #define GAPADV_PARAMS_AE_NC_NS { \
85  .eventProps = 0, \
86  .primIntMin = 160, \
87  .primIntMax = 160, \
88  .primChanMap = GAP_ADV_CHAN_ALL, \
89  .peerAddrType = PEER_ADDRTYPE_PUBLIC_OR_PUBLIC_ID, \
90  .peerAddr = { 0xaa, 0xaa, 0xaa, 0xaa, 0xaa, 0xaa }, \
91  .filterPolicy = GAP_ADV_WL_POLICY_ANY_REQ, \
92  .txPower = GAP_ADV_TX_POWER_NO_PREFERENCE, \
93  .primPhy = GAP_ADV_PRIM_PHY_1_MBPS, \
94  .secPhy = GAP_ADV_SEC_PHY_1_MBPS, \
95  .sid = 1 \
96 }
97 
98 #endif
99 
100 /*-------------------------------------------------------------------
101  * CONSTANTS
102  */
103 
157 typedef enum
158 {
167 
178 
192 
204 
213 
222 
231 
252 
264 
276 
290 
307 
309  GAP_ADV_PARAM_COUNT
319 #define GAP_ADV_INVALID_HANDLE 0xFF
321 
324 {
332 };
334 
336 typedef enum
337 {
341 
343 typedef enum
344 {
349 
351 typedef enum
352 {
367 
369 typedef enum
370 {
371  GAP_ADV_CHAN_37 = BV(0),
372  GAP_ADV_CHAN_38 = BV(1),
373  GAP_ADV_CHAN_39 = BV(2),
375  GAP_ADV_CHAN_38),
377  GAP_ADV_CHAN_39),
379  GAP_ADV_CHAN_39),
384 
386 typedef enum
387 {
408 
410 #define GAP_ADV_TX_POWER_NO_PREFERENCE 127
411 
413 typedef enum
414 {
419 
421 typedef enum
422 {
428 
436 typedef enum
437 {
441  GAP_ADV_EVT_MASK_SCAN_REQ_NOTI = AE_NOTIFY_ENABLE_SCAN_REQUEST,
449  GAP_ADV_EVT_MASK_START_AFTER_ENABLE = AE_NOTIFY_ENABLE_ADV_SET_START,
453  GAP_ADV_EVT_MASK_START = AE_NOTIFY_ENABLE_ADV_START,
457  GAP_ADV_EVT_MASK_END = AE_NOTIFY_ENABLE_ADV_END,
461  GAP_ADV_EVT_MASK_END_AFTER_DISABLE = AE_NOTIFY_ENABLE_ADV_SET_END,
472 
475  GAP_ADV_EVT_MASK_RESERVED = BV(15)
478 
483 #define GAPADV_PERIODIC_ADV_INTERVAL_MIN 0x0006
485 #define GAPADV_PERIODIC_ADV_INTERVAL_MAX 0xFFFF
487 #define GAPADV_PERIODIC_ADV_ENABLE_TX_POWER 0x0040
489 #define GAPADV_PERIODIC_ADV_DISABLE_TX_POWER 0x0000
491 #define GAPADV_PERIODIC_ADV_DATA_INTERMIDIATE_FRAG 0x00
493 #define GAPADV_PERIODIC_ADV_DATA_FIRST_FRAG 0x01
495 #define GAPADV_PERIODIC_ADV_DATA_LAST_FRAG 0x02
497 #define GAPADV_PERIODIC_ADV_DATA_COMPLETE 0x03
499 #define GAPADV_PERIODIC_ADV_MAX_DATA_LEN 252
501 
505 /*-------------------------------------------------------------------
506  * Structures
507  */
508 
521 typedef struct
522 {
523  uint16_t eventProps;
524  uint32_t primIntMin;
525  uint32_t primIntMax;
528  uint8_t peerAddr[B_ADDR_LEN];
529  GapAdv_filterPolicy_t filterPolicy;
530  int8_t txPower;
533  uint8_t sid;
535 
536 
538 typedef struct
539 {
540  uint8 handle;
541  uint8 status;
542  uint16 connHandle;
545 
547 typedef struct
548 {
549  uint8 handle;
550  uint8 scanAddrType;
551  uint8 scanAddr[B_ADDR_LEN];
552  uint8 channel;
553  int8 rssi;
555 
557 typedef struct
558 {
559  uint8 handle;
561 
564  uint16 advDataLen;
566 
568 typedef struct
569 {
574 
576 typedef struct
577 {
584  uint8 operation;
585  uint8 dataLength;
586  uint8 *pData;
588 
589 typedef struct
590 {
591  osal_event_hdr_t hdr;
592  uint8_t opcode;
593  uint8_t status;
594 } GapAdv_periodicAdvEvt_t;
595 
597 typedef struct
598 {
599  osal_event_hdr_t hdr;
600  uint8_t opcode;
601  uint8_t dataType;
602 } GapAdv_dataUpdateEvent_t;
603 
604 typedef struct
605 {
606  osal_event_hdr_t hdr;
607  uint8_t opcode;
608 } GapAv_setAdvStatusDoneEvent_t;
610 
613 /*-------------------------------------------------------------------
614  * FUNCTIONS - Advertising
615  */
616 
643 extern bStatus_t GapAdv_create(pfnGapCB_t *cb, GapAdv_params_t *advParam,
644  uint8 *advHandle);
645 
666 extern bStatus_t GapAdv_destroy(uint8 handle,
667  GapAdv_freeBufferOptions_t freeOptions);
668 
703 extern bStatus_t GapAdv_enable(uint8 handle,
704  GapAdv_enableOptions_t enableOptions,
705  uint16 durationOrMaxEvents);
706 
724 extern bStatus_t GapAdv_disable(uint8 handle);
725 
742 extern bStatus_t GapAdv_setEventMask(uint8 handle, GapAdv_eventMaskFlags_t mask);
743 
762 extern bStatus_t GapAdv_setParam(uint8 handle, GapAdv_ParamId_t paramID,
763  void *pValue);
764 
784 extern bStatus_t GapAdv_getParam(uint8 handle, GapAdv_ParamId_t paramID,
785  void *pValue, uint8_t *pLen);
786 
804 extern bStatus_t GapAdv_getBuffer(uint8 handle, GapAdv_dataTypes_t dataType,
805  uint16 *pLen, uint8 **ppBuf);
806 
866  GapAdv_freeBufferOptions_t freeOptions);
867 
912 bStatus_t GapAdv_loadByHandle(uint8 handle, GapAdv_dataTypes_t dataType,
913  uint16 len, uint8 *pBuf);
914 
953 extern bStatus_t GapAdv_prepareLoadByBuffer(uint8 *pBuf, bool freeOldData);
954 
985 extern bStatus_t GapAdv_loadByBuffer(uint16 len, uint8 *pBuf);
986 
987 
988 bStatus_t GapAdv_loadByBuffer_hook(uint16 len, uint8 *pBuf);
989 
998 extern bStatus_t GapAdv_abortLoad(void);
999 
1019 extern bStatus_t GapAdv_setVirtualAdvAddr(uint8 advHandle, uint8 *bdAddr);
1020 
1037  uint8_t GapAdv_SetPeriodicAdvParams( uint8 advHandle,
1038  GapAdv_periodicAdvParams_t *periodicAdvParams );
1039 
1056  bStatus_t GapAdv_SetPeriodicAdvData( uint8 advHandle,
1057  GapAdv_periodicAdvData_t *periodicAdvData );
1058 
1075  bStatus_t GapAdv_SetPeriodicAdvEnable( uint8 enable,
1076  uint8 advHandle );
1077 
1078 /*-------------------------------------------------------------------
1079 -------------------------------------------------------------------*/
1080 
1081 #ifdef __cplusplus
1082 }
1083 #endif
1084 
1085 #endif /* GAP_ADVERTISER_H */
1086 
uint16 periodicAdvIntervalMin
Minimum periodic advertising interval; Range: 0x0006 to 0xFFFF Time = N * 1.25 ms Time Range: 7...
Definition: gap_advertiser.h:570
Omit advertiser's address from PDU's.
Definition: gap_advertiser.h:330
uint32_t primIntMax
GAP_ADV_PARAM_PRIMARY_INTERVAL_MAX
Definition: gap_advertiser.h:525
uint8 dataLength
The number of bytes in the Advertising Data parameter.
Definition: gap_advertiser.h:585
This API allows the software components in the Z-Stack to be written independently of the specifics o...
All Channels.
Definition: gap_advertiser.h:380
GAP_Peer_Addr_Types_t
Address types used for specifying peer address type.
Definition: gap.h:727
coded-s2
Definition: gap_advertiser.h:417
uint8_t GapAdv_SetPeriodicAdvParams(uint8 advHandle, GapAdv_periodicAdvParams_t *periodicAdvParams)
Channels 37 & 39.
Definition: gap_advertiser.h:376
bStatus_t GapAdv_SetPeriodicAdvData(uint8 advHandle, GapAdv_periodicAdvData_t *periodicAdvData)
bStatus_t GapAdv_setParam(uint8 handle, GapAdv_ParamId_t paramID, void *pValue)
bStatus_t GapAdv_getParam(uint8 handle, GapAdv_ParamId_t paramID, void *pValue, uint8_t *pLen)
Definition: gap_advertiser.h:289
uint32_t primIntMin
GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN
Definition: gap_advertiser.h:524
bStatus_t GapAdv_prepareLoadByHandle(uint8 handle, GapAdv_freeBufferOptions_t freeOptions)
uint8 * pData
Periodic advertising data.
Definition: gap_advertiser.h:586
GapAdv_freeBufferOptions_t
Possible free options for Gap Advertiser API's.
Definition: gap_advertiser.h:343
Definition: gap_advertiser.h:465
1 mbps
Definition: gap_advertiser.h:415
Definition: gap_advertiser.h:221
bStatus_t GapAdv_loadByHandle(uint8 handle, GapAdv_dataTypes_t dataType, uint16 len, uint8 *pBuf)
Definition: gap_advertiser.h:331
Directed advertising.
Definition: gap_advertiser.h:327
bStatus_t GapAdv_abortLoad(void)
bStatus_t GapAdv_setVirtualAdvAddr(uint8 advHandle, uint8 *bdAddr)
Definition: gap_advertiser.h:453
bStatus_t GapAdv_enable(uint8 handle, GapAdv_enableOptions_t enableOptions, uint16 durationOrMaxEvents)
Data type returned with GAP_EVT_ADV_DATA_TRUNCATED event.
Definition: gap_advertiser.h:557
int8 rssi
RSSI of the scan req.
Definition: gap_advertiser.h:553
Scannable advertising.
Definition: gap_advertiser.h:326
uint16_t eventProps
GAP_ADV_PARAM_PROPS
Definition: gap_advertiser.h:523
Free the scan response data.
Definition: gap_advertiser.h:347
uint8 channel
Channel when the scan req was received.
Definition: gap_advertiser.h:552
GapAdv_enableOptions_t
Enable options for GapAdv_enable.
Definition: gap_advertiser.h:351
Definition: gap_advertiser.h:441
GapAdv_ParamId_t
Definition: gap_advertiser.h:157
Definition: gap_advertiser.h:392
1 mbps
Definition: gap_advertiser.h:423
uint8 handle
Advertising handle.
Definition: gap_advertiser.h:540
Definition: gap_advertiser.h:306
Don't free anything.
Definition: gap_advertiser.h:345
Definition: gap_advertiser.h:275
Channels 38 & 39.
Definition: gap_advertiser.h:378
uint16 periodicAdvIntervalMax
Maximum periodic advertising interval; Range: 0x0006 to 0xFFFF Time = N * 1.25 ms Time Range: 7...
Definition: gap_advertiser.h:571
bStatus_t GapAdv_disable(uint8 handle)
Disable an active advertising set.
void(* pfnGapCB_t)(uint32_t event, void *pBuf, uintptr_t arg)
Definition: gap.h:1343
uint8 handle
Advertising handle.
Definition: gap_advertiser.h:559
Definition: gap_advertiser.h:230
GapAdv_secondaryPHY_t secPhy
GAP_ADV_PARAM_SECONDARY_PHY
Definition: gap_advertiser.h:532
2 mbps
Definition: gap_advertiser.h:424
Scan response data.
Definition: gap_advertiser.h:339
bStatus_t GapAdv_setEventMask(uint8 handle, GapAdv_eventMaskFlags_t mask)
bStatus_t GapAdv_SetPeriodicAdvEnable(uint8 enable, uint8 advHandle)
uint16 periodicAdvProp
Periodic advertising properties - set bit 6 for include TxPower in the advertising PDU...
Definition: gap_advertiser.h:572
GapAdv_secondaryPHY_t
Gap Advertiser Options for advertising on the secondary PHY.
Definition: gap_advertiser.h:421
bStatus_t GapAdv_create(pfnGapCB_t *cb, GapAdv_params_t *advParam, uint8 *advHandle)
Definition: gap_advertiser.h:461
Definition: gap_advertiser.h:251
GapAdv_advChannels_t
GAP Advertiser Defines for Advertiser Channels.
Definition: gap_advertiser.h:369
Definition: gap_advertiser.h:191
Channels 37 & 38.
Definition: gap_advertiser.h:374
GAP_Peer_Addr_Types_t peerAddrType
GAP_ADV_PARAM_PEER_ADDRESS_TYPE
Definition: gap_advertiser.h:527
GapAdv_eventMaskFlags_t
Definition: gap_advertiser.h:436
Advertising data.
Definition: gap_advertiser.h:338
GapAdv_primaryPHY_t
Gap Advertiser Options for advertising on the primary PHY.
Definition: gap_advertiser.h:413
Definition: gap_advertiser.h:365
Type definitions and macros for BLE stack.
Channel 37.
Definition: gap_advertiser.h:371
Definition: gap_advertiser.h:177
Connectable advertising.
Definition: gap_advertiser.h:325
Free the advertising data.
Definition: gap_advertiser.h:346
Definition: gap_advertiser.h:361
bStatus_t GapAdv_getBuffer(uint8 handle, GapAdv_dataTypes_t dataType, uint16 *pLen, uint8 **ppBuf)
coded-s2
Definition: gap_advertiser.h:426
Definition: gap_advertiser.h:263
Definition: gap_advertiser.h:402
Definition: gap_advertiser.h:449
uint16 connHandle
Connection handle that ended advertising.
Definition: gap_advertiser.h:542
GAP layer interface.
OSAL Event Header.
Definition: osal.h:92
Definition: gap_advertiser.h:445
coded-s8
Definition: gap_advertiser.h:425
GapAdv_filterPolicy_t filterPolicy
GAP_ADV_PARAM_FILTER_POLICY
Definition: gap_advertiser.h:529
GapAdv_advChannels_t primChanMap
GAP_ADV_PARAM_PRIMARY_CHANNEL_MAP
Definition: gap_advertiser.h:526
Periodic advertising parameters structure.
Definition: gap_advertiser.h:568
Use legacy advertising PDU's.
Definition: gap_advertiser.h:329
GapAdv_dataTypes_t
Gap Advertising Data Types.
Definition: gap_advertiser.h:336
Definition: gap_advertiser.h:357
uint8 scanAddrType
Address type of scanning device.
Definition: gap_advertiser.h:550
uint16 advDataLen
Definition: gap_advertiser.h:564
int8_t txPower
NOT CURRENTLY IMPLEMENTED.
Definition: gap_advertiser.h:530
Data type returned with GAP_EVT_ADV_SET_TERMINATED event.
Definition: gap_advertiser.h:538
#define B_ADDR_LEN
Default Public and Random Address Length.
Definition: bcomdef.h:108
Definition: gap_advertiser.h:166
Definition: gap_advertiser.h:521
Definition: gap_advertiser.h:457
High Duty Cycle Directed Advertising.
Definition: gap_advertiser.h:328
Definition: gap_advertiser.h:397
Status_t bStatus_t
BLE Generic Status return.
Definition: bcomdef.h:251
Definition: gap_advertiser.h:406
Definition: gap_advertiser.h:212
GapAdv_filterPolicy_t
GAP Advertiser White List Policy.
Definition: gap_advertiser.h:386
bStatus_t GapAdv_prepareLoadByBuffer(uint8 *pBuf, bool freeOldData)
bStatus_t GapAdv_loadByBuffer(uint16 len, uint8 *pBuf)
Channel 39.
Definition: gap_advertiser.h:373
bStatus_t GapAdv_destroy(uint8 handle, GapAdv_freeBufferOptions_t freeOptions)
Periodic advertising data structure.
Definition: gap_advertiser.h:576
uint8 handle
Advertising handle.
Definition: gap_advertiser.h:549
GapAdv_eventProps_t
GAP Advertising Event Param Properties.
Definition: gap_advertiser.h:323
coded-s8
Definition: gap_advertiser.h:416
Data type returned with GAP_EVT_SCAN_REQ_RECEIVED event.
Definition: gap_advertiser.h:547
Channel 38.
Definition: gap_advertiser.h:372
GapAdv_primaryPHY_t primPhy
GAP_ADV_PARAM_PRIMARY_PHY
Definition: gap_advertiser.h:531
uint8_t sid
GAP_ADV_PARAM_SID
Definition: gap_advertiser.h:533
uint8 status
TODO.
Definition: gap_advertiser.h:541
uint8 numCompAdvEvts
Number of completed advertising events.
Definition: gap_advertiser.h:543
uint8 operation
Definition: gap_advertiser.h:584
Definition: gap_advertiser.h:203
uint8 availAdvDataLen
How many bytes of the advertising data were sent.
Definition: gap_advertiser.h:560
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale