rflib
Data Fields
rfc_CMD_UPDATE_RADIO_SETUP_s Struct Reference

Update Radio Settings Command. More...

#include <rf_common_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x0001. More...
 
uint16_t __dummy0
 
uint32_t * pRegOverride
 Pointer to a list of hardware and configuration registers to override. More...
 

Detailed Description

Update Radio Settings Command.

Field Documentation

§ commandNo

uint16_t rfc_CMD_UPDATE_RADIO_SETUP_s::commandNo

The command ID number 0x0001.

§ __dummy0

uint16_t rfc_CMD_UPDATE_RADIO_SETUP_s::__dummy0

§ pRegOverride

uint32_t * rfc_CMD_UPDATE_RADIO_SETUP_s::pRegOverride

Pointer to a list of hardware and configuration registers to override.


The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale