rflib
Data Fields
rfc_CMD_SET_TXSUB1_POWER_s Struct Reference

#include <rf_common_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number. More...
 
uint16_t __dummy0
 
uint32_t txSub1Power
 New TX power setting. More...
 

Field Documentation

§ commandNo

uint16_t rfc_CMD_SET_TXSUB1_POWER_s::commandNo

The command ID number.

§ __dummy0

uint16_t rfc_CMD_SET_TXSUB1_POWER_s::__dummy0

§ txSub1Power

uint32_t rfc_CMD_SET_TXSUB1_POWER_s::txSub1Power

New TX power setting.


The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale