rflib
Data Fields
rfc_CMD_SET_RAT_CPT_s Struct Reference

Set Radio Timer Channel in Capture Mode. More...

#include <rf_common_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x0603. More...
 
struct {
   uint16_t   __pad0__:3
 
   uint16_t   inputSrc:5
 Input source indicator. More...
 
   uint16_t   ratCh:4
 The radio timer channel number. More...
 
   uint16_t   bRepeated:1
 0: Single capture mode
1: Repeated capture mode More...
 
   uint16_t   inputMode:2
 Input mode:
0: Capture on rising edge
1: Capture on falling edge
2: Capture on both edges
3: Reserved More...
 
config
 
struct {
   uint16_t   __pad0__:3
 
   uint16_t   inputSrc:5
 Input source indicator. More...
 
   uint16_t   ratCh:4
 The radio timer channel number. More...
 
   uint16_t   bRepeated:1
 0: Single capture mode
1: Repeated capture mode More...
 
   uint16_t   inputMode:2
 Input mode:
0: Capture on rising edge
1: Capture on falling edge
2: Capture on both edges
3: Reserved More...
 
config
 
struct {
   uint16_t   __pad0__:3
 
   uint16_t   inputSrc:5
 Input source indicator. More...
 
   uint16_t   ratCh:4
 The radio timer channel number. More...
 
   uint16_t   bRepeated:1
 0: Single capture mode
1: Repeated capture mode More...
 
   uint16_t   inputMode:2
 Input mode:
0: Capture on rising edge
1: Capture on falling edge
2: Capture on both edges
3: Reserved More...
 
config
 

Detailed Description

Set Radio Timer Channel in Capture Mode.

Field Documentation

§ commandNo

uint16_t rfc_CMD_SET_RAT_CPT_s::commandNo

The command ID number 0x0603.

§ __pad0__

uint16_t rfc_CMD_SET_RAT_CPT_s::__pad0__

§ inputSrc

uint16_t rfc_CMD_SET_RAT_CPT_s::inputSrc

Input source indicator.

§ ratCh

uint16_t rfc_CMD_SET_RAT_CPT_s::ratCh

The radio timer channel number.

§ bRepeated

uint16_t rfc_CMD_SET_RAT_CPT_s::bRepeated

0: Single capture mode
1: Repeated capture mode

§ inputMode

uint16_t rfc_CMD_SET_RAT_CPT_s::inputMode

Input mode:
0: Capture on rising edge
1: Capture on falling edge
2: Capture on both edges
3: Reserved

§ config [1/3]

struct { ... } rfc_CMD_SET_RAT_CPT_s::config

§ config [2/3]

struct { ... } rfc_CMD_SET_RAT_CPT_s::config

§ config [3/3]

struct { ... } rfc_CMD_SET_RAT_CPT_s::config

The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale