rflib
Data Fields
rfc_CMD_PROP_SET_LEN_s Struct Reference

Set Packet Length Command. More...

#include <rf_prop_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x3401. More...
 
uint16_t rxLen
 Payload length to use. More...
 

Detailed Description

Set Packet Length Command.

Field Documentation

§ commandNo

uint16_t rfc_CMD_PROP_SET_LEN_s::commandNo

The command ID number 0x3401.

§ rxLen

uint16_t rfc_CMD_PROP_SET_LEN_s::rxLen

Payload length to use.


The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale