rflib
Data Fields
rfc_CMD_IEEE_ABORT_FG_s Struct Reference

IEEE 802.15.4 Abort Foreground Level Command. More...

#include <rf_ieee_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x2401. More...
 

Detailed Description

IEEE 802.15.4 Abort Foreground Level Command.

Field Documentation

§ commandNo

uint16_t rfc_CMD_IEEE_ABORT_FG_s::commandNo

The command ID number 0x2401.


The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale