rflib
Data Fields
RF_Params Struct Reference

RF driver configuration parameters. More...

#include <RFCC26X2.h>

Collaboration diagram for RF_Params:
Collaboration graph
[legend]

Data Fields

uint32_t nInactivityTimeout
 
uint32_t nPowerUpDuration
 
RF_Callback pPowerCb
 
RF_Callback pErrCb
 
uint16_t nPowerUpDurationMargin
 
uint16_t nPhySwitchingDurationMargin
 An additional safety margin to be used to calculate when conflicts shall be evaluated run-time. More...
 
RF_ClientCallback pClientEventCb
 
RF_ClientEventMask nClientEventMask
 
uint32_t nID
 RF handle identifier. More...
 

Detailed Description

RF driver configuration parameters.

RF_Params is used for initial RF driver configuration. It is initialized by RF_Params_init() and used by RF_open(). Each client has its own set of parameters. They are reconfigured on a client switch. Some of the parameters can be changed during run-time using RF_control().

Field Documentation

§ nInactivityTimeout

uint32_t RF_Params::nInactivityTimeout

Inactivity timeout in microseconds. The default value is 0xFFFFFFFF (infinite).

§ nPowerUpDuration

uint32_t RF_Params::nPowerUpDuration

A custom power-up duration in microseconds. If 0, the RF driver will start with a conservative value and measure the actual time during the first power-up. The default value is 0.

§ pPowerCb

RF_Callback RF_Params::pPowerCb
Deprecated:
Power up callback, will be removed future versions, see RF_Params::pClienteventCb instead. The default value is NULL.

§ pErrCb

RF_Callback RF_Params::pErrCb
Deprecated:
Callback function for driver error events.

§ nPowerUpDurationMargin

uint16_t RF_Params::nPowerUpDurationMargin

An additional safety margin to be added to RF_Params::nPowerUpDuration. This is necessary because of other hardware and software interrupts preempting the RF driver interrupt handlers and state machine. The default value is platform-dependent.

§ nPhySwitchingDurationMargin

uint16_t RF_Params::nPhySwitchingDurationMargin

An additional safety margin to be used to calculate when conflicts shall be evaluated run-time.

§ pClientEventCb

RF_ClientCallback RF_Params::pClientEventCb

Callback function for client-related events. The default value is NULL.

§ nClientEventMask

RF_ClientEventMask RF_Params::nClientEventMask

Event mask used to subscribe certain client events. The purpose is to keep the number of callback executions small.

§ nID

uint32_t RF_Params::nID

RF handle identifier.


The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale