Data Fields
SPICC26X4DMA_HWAttrs Struct Reference

SPICC26X4DMA Hardware attributes. More...

#include <SPICC26X4DMA.h>

Data Fields

uint32_t baseAddr
 SPI Peripheral's base address. More...
 
uint8_t intNum
 
uint8_t intPriority
 SPI CC26X4DMA Peripheral's interrupt priority. More...
 
uint32_t swiPriority
 SPI SWI priority. The higher the number, the higher the priority. The minimum is 0 and the maximum is 15 by default. The maximum can be reduced to save RAM by adding or modifying Swi.numPriorities in the kernel configuration file. More...
 
PowerCC26XX_Resource powerMngrId
 
uint16_t defaultTxBufValue
 
uint32_t rxChannelBitMask
 
uint32_t txChannelBitMask
 
volatile tDMAControlTable * dmaTxTableEntryPri
 
volatile tDMAControlTable * dmaRxTableEntryPri
 
volatile tDMAControlTable * dmaTxTableEntryAlt
 
volatile tDMAControlTable * dmaRxTableEntryAlt
 
int32_t txPinMux
 
int32_t rxPinMux
 
int32_t clkPinMux
 
int32_t csnPinMux
 
uint_least8_t picoPin
 
uint_least8_t pociPin
 
uint_least8_t clkPin
 
uint_least8_t csnPin
 
uint32_t minDmaTransferSize
 

Detailed Description

SPICC26X4DMA Hardware attributes.

These fields, with the exception of intPriority, are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For CC26x4Ware these definitions are found in:

intPriority is the SPI peripheral's interrupt priority, as defined by the underlying OS. It is passed unmodified to the underlying OS's interrupt handler creation code, so you need to refer to the OS documentation for usage. For example, for SYS/BIOS applications, refer to the ti.sysbios.family.arm.m3.Hwi documentation for SYS/BIOS usage of interrupt priorities. If the driver uses the ti.dpl interface instead of making OS calls directly, then the HwiP port handles the interrupt priority in an OS specific way. In the case of the SYS/BIOS port, intPriority is passed unmodified to Hwi_create().

A sample structure is shown below:

const SPICC26X4DMA_HWAttrs SPICC26X4DMAobjects[] = {
{
.baseAddr = SPI0_BASE,
.intNum = INT_SPI0,
.intPriority = ~0,
.swiPriority = 0,
.powerMngrId = PERIPH_SPI0,
.defaultTxBufValue = 0,
.rxChannelBitMask = UDMA_CHAN_SPI0_RX,
.txChannelBitMask = UDMA_CHAN_SPI0_TX,
.picoPin = CONFIG_SPI0_POCI,
.pociPin = CONFIG_SPI0_PICO,
.clkPin = CONFIG_SPI0_CLK,
.csnPin = CONFIG_SPI0_CSN
},
{
.baseAddr = SPI1_BASE,
.intNum = INT_SPI1,
.intPriority = ~0,
.swiPriority = 0,
.powerMngrId = PERIPH_SPI1,
.defaultTxBufValue = 0,
.rxChannelBitMask = UDMA_CHAN_SPI1_RX,
.txChannelBitMask = UDMA_CHAN_SPI1_TX,
.picoPin = CONFIG_SPI1_POCI,
.pociPin = CONFIG_SPI1_PICO,
.clkPin = CONFIG_SPI1_CLK,
.csnPin = CONFIG_SPI1_CSN
},
};

Field Documentation

§ baseAddr

uint32_t SPICC26X4DMA_HWAttrs::baseAddr

SPI Peripheral's base address.

§ intNum

uint8_t SPICC26X4DMA_HWAttrs::intNum

SPI CC26X4DMA Peripheral's interrupt vector

§ intPriority

uint8_t SPICC26X4DMA_HWAttrs::intPriority

SPI CC26X4DMA Peripheral's interrupt priority.

The CC26x4 uses three of the priority bits, meaning ~0 has the same effect as (7 << 5).

(7 << 5) will apply the lowest priority.

(1 << 5) will apply the highest priority.

Setting the priority to 0 is not supported by this driver.

HWI's with priority 0 ignore the HWI dispatcher to support zero-latency interrupts, thus invalidating the critical sections in this driver.

§ swiPriority

uint32_t SPICC26X4DMA_HWAttrs::swiPriority

SPI SWI priority. The higher the number, the higher the priority. The minimum is 0 and the maximum is 15 by default. The maximum can be reduced to save RAM by adding or modifying Swi.numPriorities in the kernel configuration file.

§ powerMngrId

PowerCC26XX_Resource SPICC26X4DMA_HWAttrs::powerMngrId

SPI Peripheral's power manager ID

§ defaultTxBufValue

uint16_t SPICC26X4DMA_HWAttrs::defaultTxBufValue

Default TX value if txBuf == NULL

§ rxChannelBitMask

uint32_t SPICC26X4DMA_HWAttrs::rxChannelBitMask

uDMA controlTable channel index

§ txChannelBitMask

uint32_t SPICC26X4DMA_HWAttrs::txChannelBitMask

uDMA controlTable channel index

§ dmaTxTableEntryPri

volatile tDMAControlTable* SPICC26X4DMA_HWAttrs::dmaTxTableEntryPri

uDMA controlTable primary tx entry

§ dmaRxTableEntryPri

volatile tDMAControlTable* SPICC26X4DMA_HWAttrs::dmaRxTableEntryPri

uDMA controlTable primary tx entry

§ dmaTxTableEntryAlt

volatile tDMAControlTable* SPICC26X4DMA_HWAttrs::dmaTxTableEntryAlt

uDMA controlTable alternate tx entry

§ dmaRxTableEntryAlt

volatile tDMAControlTable* SPICC26X4DMA_HWAttrs::dmaRxTableEntryAlt

uDMA controlTable alternate rx entry

§ txPinMux

int32_t SPICC26X4DMA_HWAttrs::txPinMux

Tx PIN mux value. Can be applied to either PICO or POCI

§ rxPinMux

int32_t SPICC26X4DMA_HWAttrs::rxPinMux

Rx PIN mux value. Can be applied to either PICO or POCI

§ clkPinMux

int32_t SPICC26X4DMA_HWAttrs::clkPinMux

CLK PIN mux value for flow control

§ csnPinMux

int32_t SPICC26X4DMA_HWAttrs::csnPinMux

CSN PIN mux value for flow control

§ picoPin

uint_least8_t SPICC26X4DMA_HWAttrs::picoPin

SPI PICO pin

§ pociPin

uint_least8_t SPICC26X4DMA_HWAttrs::pociPin

SPI POCI pin

§ clkPin

uint_least8_t SPICC26X4DMA_HWAttrs::clkPin

SPI CLK pin

§ csnPin

uint_least8_t SPICC26X4DMA_HWAttrs::csnPin

SPI CSN pin

§ minDmaTransferSize

uint32_t SPICC26X4DMA_HWAttrs::minDmaTransferSize

Minimum transfer size for DMA based transfer


The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale