|
void | SPIConfigSetExpClk (uint32_t ui32Base, uint32_t ui32SPIClk, uint32_t ui32Protocol, uint32_t ui32Mode, uint32_t ui32BitRate, uint32_t ui32DataWidth) |
| Configures the serial peripheral port. More...
|
|
int32_t | SPIDataPutNonBlocking (uint32_t ui32Base, uint32_t ui32Data) |
| Puts a data element into the SPI transmit FIFO. More...
|
|
void | SPIDataPut (uint32_t ui32Base, uint32_t ui32Data) |
| Puts a data element into the SPI transmit FIFO. More...
|
|
void | SPIDataGet (uint32_t ui32Base, uint32_t *pui32Data) |
| Gets a data element from the SPI receive FIFO. More...
|
|
int32_t | SPIDataGetNonBlocking (uint32_t ui32Base, uint32_t *pui32Data) |
| Gets a data element from the SPI receive FIFO. More...
|
|
static uint32_t | SPIIntNumberGet (uint32_t ui32Base) |
|
void | SPIIntRegister (uint32_t ui32Base, void(*pfnHandler)(void)) |
| Registers an interrupt handler for the Serial Peripheral Interface in the dynamic interrupt table. More...
|
|
void | SPIIntUnregister (uint32_t ui32Base) |
| Unregisters an interrupt handler for the Serial Peripheral Interface in the dynamic interrupt table. More...
|
|