![]() |
![]() |
|
Z-Stack API Reference
7.10.00.08
|
This group defines the server commands received (Client-to-Server in ZCL Header) defined in the ZCL v7 specification. More...
Macros | |
| #define | COMMAND_IASWD_START_WARNING 0x00 |
| #define | COMMAND_IASWD_SQUAWK 0x01 |
This group defines the server commands received (Client-to-Server in ZCL Header) defined in the ZCL v7 specification.
| #define COMMAND_IASWD_SQUAWK 0x01 |
This command uses the WD capabilities to emit a quick audible/visible pulse called a "squawk". The squawk command has no effect if the WD is currently active (warning in progress).
| #define COMMAND_IASWD_START_WARNING 0x00 |
This command starts the WD operation. The WD alerts the surrounding area by audible (siren) and visual (strobe) signals.