![]() |
![]() |
|
Z-Stack API Reference
7.10.00.08
|
This group provides ZCL Closure Shade Config Cluster macros defined in the ZCL v7 specification. More...
Macros | |
| #define | ATTRID_SHADE_CONFIGURATION_PHYSICAL_CLOSED_LIMIT 0x0000 |
| #define | ATTRID_SHADE_CONFIGURATION_MOTOR_STEP_SIZE 0x0001 |
| #define | ATTRID_SHADE_CONFIGURATION_STATUS 0x0002 |
| The Status attribute indicates the status of a number of shade functions. | |
| #define | CLOSURES_STATUS_SHADE_IS_OPERATIONAL 0x01 |
| Shade operational if set. | |
| #define | CLOSURES_STATUS_SHADE_IS_ADJUSTING 0x02 |
| Shade adjusting if set. | |
| #define | CLOSURES_STATUS_SHADE_DIRECTION 0x04 |
| Shade direction opening if set. | |
| #define | CLOSURES_STATUS_SHADE_MOTOR_FORWARD_DIRECTION 0x08 |
| Direction corresponding to forward direction of motor, opening if set. | |
| #define | ATTRID_SHADE_CONFIGURATION_CLOSED_LIMIT 0x0010 |
| #define | ATTRID_SHADE_CONFIGURATION_MODE 0x0011 |
| The Mode attribute indicates the current operating mode of the shade. | |
| #define | CLOSURES_MODE_NORMAL_MODE 0x00 |
| #define | CLOSURES_MODE_CONFIGURE_MODE 0x01 |
| #define | ZCL_CLOSURES_LOGICAL_CLUSTER_ID_SHADE_CONFIG 0x0010 |
This group provides ZCL Closure Shade Config Cluster macros defined in the ZCL v7 specification.
| #define ATTRID_SHADE_CONFIGURATION_CLOSED_LIMIT 0x0010 |
The ClosedLimit attribute indicates the most closed position that the shade can move to.
| #define ATTRID_SHADE_CONFIGURATION_MOTOR_STEP_SIZE 0x0001 |
The MotorStepSize attribute indicates the angle the shade motor moves for one step, measured in 1/10ths of a degree.
| #define ATTRID_SHADE_CONFIGURATION_PHYSICAL_CLOSED_LIMIT 0x0000 |
The PhysicalClosedLimit attribute indicates the most closed (numerically lowest) position that the shade can physically move to.
| #define ZCL_CLOSURES_LOGICAL_CLUSTER_ID_SHADE_CONFIG 0x0010 |
The ClosedLimit attribute indicates the most closed position that the shade can move to.