#include <DisplaySharp.h>
§ spiIndex
uint32_t DisplaySharp_HWAttrsV1::spiIndex |
§ csPin
uint32_t DisplaySharp_HWAttrsV1::csPin |
§ powerPin
uint32_t DisplaySharp_HWAttrsV1::powerPin |
§ enablePin
uint32_t DisplaySharp_HWAttrsV1::enablePin |
§ pixelHeight
uint16_t DisplaySharp_HWAttrsV1::pixelHeight |
§ pixelWidth
uint16_t DisplaySharp_HWAttrsV1::pixelWidth |
§ displayBuf
void* DisplaySharp_HWAttrsV1::displayBuf |
§ font
const Graphics_Font* DisplaySharp_HWAttrsV1::font |
The documentation for this struct was generated from the following file: