Macros | |
#define | UART2_STATUS_SUCCESS (0) |
Successful status code returned by UART2 APIs. More... | |
#define | UART2_STATUS_SREADTIMEOUT (1) |
A read timeout occurred (not an error). More... | |
#define | UART2_STATUS_EFRAMING (-1) |
A framing error occurred. More... | |
#define | UART2_STATUS_EPARITY (-2) |
A parity error occurred. More... | |
#define | UART2_STATUS_EBREAK (-4) |
A break error occurred. More... | |
#define | UART2_STATUS_EOVERRUN (-8) |
A FIFO overrun occurred. More... | |
#define | UART2_STATUS_EINUSE (-9) |
The UART is currently in use. More... | |
#define | UART2_STATUS_EINVALID (-10) |
An invalid argument or UART2_Params field was passed to UART2 API. More... | |
#define | UART2_STATUS_EFAIL (-11) |
General failure status returned by UART2 API. More... | |
#define | UART2_STATUS_EMEMORY (-12) |
A memory allocation failure occurred. More... | |
#define | UART2_STATUS_ETIMEOUT (-13) |
A timeout occurred for a blocking UART2_read or UART2_write call. More... | |
#define | UART2_STATUS_ECANCELLED (-14) |
A UART2_write() or UART2_read() operation was cancelled. More... | |
#define | UART2_STATUS_ENOTOPEN (-15) |
A UART2_write() or UART2_read() called on a device not opened. More... | |
#define | UART2_STATUS_EAGAIN (-16) |
A UART2_write() or UART2_read() in UART2_Mode_NONBLOCKING would have blocked. More... | |
#define UART2_STATUS_SUCCESS (0) |
Successful status code returned by UART2 APIs.
#define UART2_STATUS_SREADTIMEOUT (1) |
A read timeout occurred (not an error).
#define UART2_STATUS_EFRAMING (-1) |
A framing error occurred.
#define UART2_STATUS_EPARITY (-2) |
A parity error occurred.
#define UART2_STATUS_EBREAK (-4) |
A break error occurred.
#define UART2_STATUS_EOVERRUN (-8) |
A FIFO overrun occurred.
#define UART2_STATUS_EINUSE (-9) |
The UART is currently in use.
#define UART2_STATUS_EINVALID (-10) |
An invalid argument or UART2_Params field was passed to UART2 API.
#define UART2_STATUS_EFAIL (-11) |
General failure status returned by UART2 API.
#define UART2_STATUS_EMEMORY (-12) |
A memory allocation failure occurred.
#define UART2_STATUS_ETIMEOUT (-13) |
A timeout occurred for a blocking UART2_read or UART2_write call.
#define UART2_STATUS_ECANCELLED (-14) |
A UART2_write() or UART2_read() operation was cancelled.
#define UART2_STATUS_ENOTOPEN (-15) |
A UART2_write() or UART2_read() called on a device not opened.
#define UART2_STATUS_EAGAIN (-16) |
A UART2_write() or UART2_read() in UART2_Mode_NONBLOCKING would have blocked.