Migrating to a secure environment¶
The following section covers the steps required to migrate a non-secure example to one that leverages security through Arm TrustZone on CC13x4 or CC26x4.
Two approaches are presented. The first method consists in leveraging a TI-provided project with Trusted Firmware-M (TF-M) implemented. The second method leads you to modify any CC13x4 or CC26x4 project to enable TF-M.
The first approach (project migration) is recommended when a TF-M version
of the example used as base for your project is available in the SDK.
For example, if your project is based on the empty
example, you migrate
your code into the tfm_empty
example.
The second approach (consisting in enabling TF-M on an existing project) is applicable on all the CC13x4 or CC26x4 projects.
Project migration¶
Identify the differences between your project and the unmodified example project in the SDK. These differences include the created files, the altered project configurations, the modified and the changes made in the linker command file. The SysConfig configurations are usually contained in
.syscfg
files. The linker command file is named differently according to the toolchain used (.cmd
for TIClang,.ipcf
for IAR or .``lds`` for GCC).Import the unmodified TF-M version of the example in your development environment (i.e. CCS or IAR).
Implement the differences identified at step #1. Created files can directly be copy-pasted into the newly created project. However, it is recommended to apply the changes in the project configuration, SysConfig and the linker command file line by line to avoid unintentional alteration of the project.
Enable Trusted Firmware-M on an existing project¶
Several modifications are required in a TF-M disabled project in order to enable TF-M. These modifications should ensure the proper secure software components (secure image, veneers, drivers) are selected and linked. From the developer’s point of view, modifications are required in SysConfig, the Project configuration and in the linker command file.
SysConfig¶
When configured to do so, SysConfig ensures
The secured-implementation of the crypto drivers is used to build the application
The linker is configured to use the veneers library
Configuring SysConfig to do so takes to enable TrustZone
:
Open the SysConfig file (
.syscfg
)Under
TI UTILS
, enableTrustZone

Figure 231. Enable “TrustZone” using SysConfig¶
One can review the files generated by SysConfig (especially
ti_drivers_config.c
and ti_utils_build_linker.cmd.genlibs
)
and notice the secure driver, secure driver library and
veneers are used by the project when TrustZone is enabled.
Project configuration¶
The project configuration ensures the toolchain (compiler and linker) have the right options, especially when it comes to the predefined symbols and included libraries. The project configuration can be modified by accessing the project properties from your IDE.
- Add the following predefined symbols
TFM_ENABLED=1
MBEDTLS_CONFIG_FILE="<configs/config-tidrivers.h>"
- Add the following include path to the compiler
${COM_TI_SIMPLELINK_CC13XX_CC26XX_SDK_INSTALL_DIR}/source/third_party/tfm/interface/include
- Add the following library include to the linker
${COM_TI_SIMPLELINK_CC13XX_CC26XX_SDK_INSTALL_DIR}/tfm_s
Linker commmand file¶
The linker command file should ensure
The secure image is linked at address
0x00000000
. The rest of the flash is for non-secure code.The starting address of application matches the base address of the non-secure application base address defined in the in the TF-M memory layouts.
A part of the RAM is reserved for secure operations (the rest of the RAM is for non-secure operations).
To do so, in the linker command file (.cmd
for TIClang, .ipcf
for IAR
or .lds
for GCC compiler), modify the following elements:
Set the Flash origin and Flash size / Flash end for the application considering the Flash used by the secure image and secure boot.
The starting address of the non-secure application is given by the TF-M memory layouts. The starting address of the non-secure application is
0x00038100
by default.The Flash length should be set to
0xC6F00
and/or the Flash end should be set to0x000FEFFF
. This is to ensure0x1000
bytes of Flash is left for the Secure Boot.
For TIClang
Assuming you are using TIClang toolchain, the following symbols should be changed in the linker command file (
.cmd
)./* #define FLASH_BASE 0x0 #define FLASH_SIZE 0x100000 #define RAM_BASE 0x20000000 #define RAM_SIZE 0x40000 */ #define FLASH_S_BASE 0x0 #define FLASH_SCSIZE 0x38000 #define FLASH_BASE 0x00038100 #define FLASH_SIZE 0xC6F00 #define RAM_BASE 0x2000C000 #define RAM_SIZE 0x30000
For IAR
Assuming you are using IAR toolchain, the following symbols should be changed in the linker command file (
.ipcf
)./* define symbol ROM_start__ = 0x00000000; define symbol ROM_end__ = 0x000FFFFF; define symbol RAM_start__ = 0x20000000; define symbol __intvec_start__ = 0x00000000; */ define symbol ROM_start__ = 0x00038100; define symbol ROM_end__ = 0x000FEFFF; define symbol RAM_start__ = 0x2000C000; define symbol __intvec_start__ = 0x00038100;
For GCC
Assuming you are using GCC toolchain, the following symbols should be changed in the linker command file (
.lds
)./* FLASH (RX) : ORIGIN = 0x00000000, LENGTH = 0x000FFFFF */ FLASH (RX) : ORIGIN = 0x00038100, LENGTH = 0x000C6F00 /* SRAM (RWX) : ORIGIN = 0x20000000, LENGTH = 0x00040000 */ SEC_SRAM (RWX) : ORIGIN = 0x20000000, LENGTH = 0x0000C000 SRAM (RWX) : ORIGIN = 0x2000C000, LENGTH = 0x00034000 /* .resetVecs (0x0) : AT (0x0) { */ .resetVecs (0x00038100) : AT (0x00038100) { /* UDMACC26XX_CONFIG_BASE = 0x20000400; */ UDMACC26XX_CONFIG_BASE = 0x2000C400;
Ensures the interrupt vectors is linked at 256-byte boundry closest to NS flash base (i.e. at
0x00038100
)Set the RAM origin and RAM size for the application considering the RAM used by the secure image.
The RAM base (RAM base) should be set to
0x2000C000
as the RAM starts at0x20000000
and the secure image uses by default0x0000C000
bytes of RAM.The remaining RAM size (
0x34000
) is usable by the application (i.e. the RAM end can be left as it,0x2003FFFF
).
Review one more time the linker command file to make sure nothing is linked at the addresses used by the secure image