TI OAD API Documentation
2.02.08.00
|
Macros | |
#define | OAD_IMG_TYPE_APP 1 |
#define | OAD_IMG_TYPE_APP_STACK 3 |
#define | OAD_IMG_TYPE_APPSTACKLIB 7 |
#define | OAD_IMG_TYPE_BIM 6 |
#define | OAD_IMG_TYPE_FACTORY 5 |
#define | OAD_IMG_TYPE_NP 4 |
#define | OAD_IMG_TYPE_PERSISTENT_APP 0 |
#define | OAD_IMG_TYPE_RSVD_BEGIN 64 |
#define | OAD_IMG_TYPE_RSVD_END 255 |
#define | OAD_IMG_TYPE_STACK 2 |
#define OAD_IMG_TYPE_APP 1 |
OAD user application image
A user application of split app/stack type
#define OAD_IMG_TYPE_APP_STACK 3 |
OAD app + stack merge
An OAD enabled image that is a merge of both app and stack that are of split image type.
#define OAD_IMG_TYPE_APPSTACKLIB 7 |
OAD app + stack library image
An OAD enabled executable where the app and stack are built and linked together as one image.
#define OAD_IMG_TYPE_BIM 6 |
OAD Boot Image Manager (BIM) image
A BIM image
#define OAD_IMG_TYPE_FACTORY 5 |
OAD network processor image
A network processor image. This image is intended to run an external processor
#define OAD_IMG_TYPE_NP 4 |
OAD network processor image
A network processor image. This image is intended to run an external processor
#define OAD_IMG_TYPE_PERSISTENT_APP 0 |
OAD on-chip persistent application image
The persistent app is the permanently resident app used in on-chip OAD The persistent app is responsible for updating the user application
#define OAD_IMG_TYPE_RSVD_BEGIN 64 |
OAD reserved image type begin
#define OAD_IMG_TYPE_RSVD_END 255 |
OAD reserved image type end
#define OAD_IMG_TYPE_STACK 2 |
OAD stack image
An OAD enabled stack image of split image type