![]() |
![]() |
|
Z-Stack API Reference
6.30.00.23
|
#include <zstack.h>
Data Fields | |
| uint8_t | logicalChannel |
| uint16_t | panID |
| zstack_LongAddr_t | extendedPANID |
| uint16_t | chosenParent |
| uint8_t | parentDepth |
| uint8_t | stackProfile |
Structure to send a Device Join Requst.
| uint16_t chosenParent |
Short address of parent device chosen to join
| zstack_LongAddr_t extendedPANID |
64 bit extended PAN ID, use all 0xFF if don't care
| uint8_t logicalChannel |
Channel where the PAN is located
| uint16_t panID |
ID of the PAN to join
| uint8_t parentDepth |
Depth of the parent
| uint8_t stackProfile |
Stack profile of the network to join