![]() |
![]() |
|
Z-Stack API Reference
6.30.00.23
|
This group provides ZCL Closure Windo Covering Cluster macros defined in the ZCL v7 specification. More...
Macros | |
| #define | ATTRSET_WINDOW_COVERING_INFO 0x0000 |
| #define | ATTRSET_WINDOW_COVERING_SETTINGS 0x0010 |
| #define | ATTRID_WINDOW_COVERING_WINDOW_COVERING_TYPE 0x0000 |
| #define | ATTRID_WINDOW_COVERING_PHYSICAL_CLOSED_LIMIT_LIFT 0x0001 |
| #define | ATTRID_WINDOW_COVERING_PHYSICAL_CLOSED_LIMIT_TILT 0x0002 |
| #define | ATTRID_WINDOW_COVERING_CURRENT_POSITION_LIFT 0x0003 |
| #define | ATTRID_WINDOW_COVERING_CURRENT_POSITION_TILT 0x0004 |
| #define | ATTRID_WINDOW_COVERING_NUMBER_OF_ACTUATIONS_LIFT 0x0005 |
| #define | ATTRID_WINDOW_COVERING_NUMBER_OF_ACTUATIONS_TILT 0x0006 |
| #define | ATTRID_WINDOW_COVERING_CONFIG_OR_STATUS 0x0007 |
| The ConfigStatus attribute makes configuration and status information available. | |
| #define | ATTRID_WINDOW_COVERING_CURRENT_POSITION_LIFT_PERCENTAGE 0x0008 |
| #define | ATTRID_WINDOW_COVERING_CURRENT_POSITION_TILT_PERCENTAGE 0x0009 |
| #define | ATTRID_WINDOW_COVERING_INSTALLED_OPEN_LIMIT_LIFT 0x0010 |
| #define | ATTRID_WINDOW_COVERING_INSTALLED_CLOSED_LIMIT_LIFT 0x0011 |
| #define | ATTRID_WINDOW_COVERING_INSTALLED_OPEN_LIMIT_TILT 0x0012 |
| #define | ATTRID_WINDOW_COVERING_INSTALLED_CLOSED_LIMIT_TILT 0x0013 |
| #define | ATTRID_WINDOW_COVERING_VELOCITY_LIFT 0x0014 |
| #define | ATTRID_WINDOW_COVERING_ACCELERATION_TIME_LIFT 0x0015 |
| #define | ATTRID_WINDOW_COVERING_DECELERATION_TIME_LIFT 0x0016 |
| #define | ATTRID_WINDOW_COVERING_MODE 0x0017 |
| The Mode attribute allows configuration of the Window Covering. | |
| #define | ATTRID_WINDOW_COVERING_INTERMEDIATE_SETPOINTS_LIFT 0x0018 |
| #define | ATTRID_WINDOW_COVERING_INTERMEDIATE_SETPOINTS_TILT 0x0019 |
| #define | CLOSURES_WINDOW_COVERING_TYPE_ROLLERSHADE 0x00 |
| Window Covering Type enum. | |
| #define | CLOSURES_WINDOW_COVERING_TYPE_ROLLERSHADE_2_MOTOR 0x01 |
| #define | CLOSURES_WINDOW_COVERING_TYPE_ROLLERSHADE_EXTERIOR 0x02 |
| #define | CLOSURES_WINDOW_COVERING_TYPE_ROLLERSHADE_EXTERIOR_2_MOTOR 0x03 |
| #define | CLOSURES_WINDOW_COVERING_TYPE_DRAPERY 0x04 |
| #define | CLOSURES_WINDOW_COVERING_TYPE_AWNING 0x05 |
| #define | CLOSURES_WINDOW_COVERING_TYPE_SHUTTER 0x06 |
| #define | CLOSURES_WINDOW_COVERING_TYPE_TILT_BLIND_TILT_ONLY 0x07 |
| #define | CLOSURES_WINDOW_COVERING_TYPE_TILT_BLIND_LIFT_AND_TILT 0x08 |
| #define | CLOSURES_WINDOW_COVERING_TYPE_PROJECTOR_SCREEN 0x09 |
| #define | COMMAND_WINDOW_COVERING_UP_OR_OPEN ( 0x00 ) |
| #define | COMMAND_WINDOW_COVERING_DOWN_OR_CLOSE ( 0x01 ) |
| #define | COMMAND_WINDOW_COVERING_STOP ( 0x02 ) |
| #define | COMMAND_WINDOW_COVERING_GO_TO_LIFT_VALUE ( 0x04 ) |
| #define | COMMAND_WINDOW_COVERING_GO_TO_LIFT_PERCENTAGE ( 0x05 ) |
| #define | COMMAND_WINDOW_COVERING_GO_TO_TILT_VALUE ( 0x07 ) |
| #define | COMMAND_WINDOW_COVERING_GO_TO_TILT_PERCENTAGE ( 0x08 ) |
| #define | ZCL_WC_GOTOVALUEREQ_PAYLOADLEN ( 2 ) |
| #define | ZCL_WC_GOTOPERCENTAGEREQ_PAYLOADLEN ( 1 ) |
This group provides ZCL Closure Windo Covering Cluster macros defined in the ZCL v7 specification.
| #define ATTRID_WINDOW_COVERING_ACCELERATION_TIME_LIFT 0x0015 |
The AccelerationTimeLift attribute identifies any ramp up times to reaching the velocity setting (in tenth of a second) for positioning the Window Covering.
| #define ATTRID_WINDOW_COVERING_CURRENT_POSITION_LIFT 0x0003 |
The CurrentPositionLift attribute identifies the actual position (in centimeters) of the window covering from the top of the shade if Closed Loop Control is enabled. This attribute is ignored if the device is running in Open Loop Control.
| #define ATTRID_WINDOW_COVERING_CURRENT_POSITION_LIFT_PERCENTAGE 0x0008 |
The CurrentPositionLiftPercentage attribute identifies the actual position as a percentage between the InstalledOpenLimitLift attribute and the InstalledClosedLimitLift attribute of the window covering from the up/open position if Closed Loop Control is enabled.
| #define ATTRID_WINDOW_COVERING_CURRENT_POSITION_TILT 0x0004 |
The NumberOfActuationsTilt attribute identifies the total number of tilt actuations applied to the Window Covering since the device was installed.
| #define ATTRID_WINDOW_COVERING_CURRENT_POSITION_TILT_PERCENTAGE 0x0009 |
The CurrentPositionTiltPercentage attribute identifies the actual position as a percentage between the InstalledOpenLimitTilt attribute and the InstalledClosedLimitTilt attribute of the window covering from the up/open position if Closed Loop Control is enabled.
| #define ATTRID_WINDOW_COVERING_DECELERATION_TIME_LIFT 0x0016 |
The DecelerationTimeLift attribute identifies any ramp down times associated with stopping the positioning (in tenth of a second) of the Window Covering.
| #define ATTRID_WINDOW_COVERING_INSTALLED_CLOSED_LIMIT_LIFT 0x0011 |
The InstalledClosedLimitLift attribute identifies the Closed Limit for Lifting the Window Covering whether position (in centimeters) is encoded or timed.
| #define ATTRID_WINDOW_COVERING_INSTALLED_CLOSED_LIMIT_TILT 0x0013 |
The InstalledClosedLimitTilt attribute identifies the Closed Limit for Tilting the Window Covering whether position (in tenth of a degree) is encoded or timed.
| #define ATTRID_WINDOW_COVERING_INSTALLED_OPEN_LIMIT_LIFT 0x0010 |
The InstalledOpenLimitLift attribute identifies the Open Limit for Lifting the Window Covering whether position (in centimeters) is encoded or timed.
| #define ATTRID_WINDOW_COVERING_INSTALLED_OPEN_LIMIT_TILT 0x0012 |
The InstalledOpenLimitTilt attribute identifies the Open Limit for Tilting the Window Covering whether position (in tenth of a degree) is encoded or timed.
| #define ATTRID_WINDOW_COVERING_INTERMEDIATE_SETPOINTS_LIFT 0x0018 |
Identifies the number of Intermediate Setpoints supported by the Window Covering for Lift and then identifies the position settings for those Intermediate Setpoints if Closed Loop Control is supported.
| #define ATTRID_WINDOW_COVERING_INTERMEDIATE_SETPOINTS_TILT 0x0019 |
Identifies the number of Intermediate Setpoints supported by the Window Covering for Tilt and then identifies the position settings for those Intermediate Setpoints if Closed Loop Control is supported.
| #define ATTRID_WINDOW_COVERING_NUMBER_OF_ACTUATIONS_LIFT 0x0005 |
The NumberOfActuationsLift attribute identifies the total number of lift actuations applied to the Window Covering since the device was installed.
| #define ATTRID_WINDOW_COVERING_NUMBER_OF_ACTUATIONS_TILT 0x0006 |
The NumberOfActuationsTilt attribute identifies the total number of tilt actuations applied to the Window Covering since the device was installed.
| #define ATTRID_WINDOW_COVERING_PHYSICAL_CLOSED_LIMIT_LIFT 0x0001 |
The PhysicalClosedLimitLift attribute identifies the maximum possible encoder position possible (in centimeters) to position the height of the window covering - this is ignored if the device is running in Open Loop Control.
| #define ATTRID_WINDOW_COVERING_PHYSICAL_CLOSED_LIMIT_TILT 0x0002 |
The PhysicalClosedLimitTilt attribute identifies the maximum possible encoder position possible (tenth of a degrees) to position the angle of the window covering - this is ignored if the device is running in Open Loop Control.
| #define ATTRID_WINDOW_COVERING_VELOCITY_LIFT 0x0014 |
The VelocityLift attribute identifies the velocity (in centimeters per second) associated with Lifting the Window Covering.
| #define ATTRID_WINDOW_COVERING_WINDOW_COVERING_TYPE 0x0000 |
The WindowCoveringType attribute identifies the type of window covering being controlled by this endpoint
| #define COMMAND_WINDOW_COVERING_DOWN_OR_CLOSE ( 0x01 ) |
Upon receipt of this command, the Window Covering will adjust the window so the physical lift is at the InstalledClosedLimit - Lift and the tilt is at the InstalledClosedLimit - Tilt. This will happen as fast as possible.
| #define COMMAND_WINDOW_COVERING_GO_TO_LIFT_PERCENTAGE ( 0x05 ) |
Upon receipt of this command, the Window Covering will adjust the window so the physical lift is at the lift percentage specified in the payload of this command.
| #define COMMAND_WINDOW_COVERING_GO_TO_LIFT_VALUE ( 0x04 ) |
Upon receipt of this command, the Window Covering will adjust the window so the physical lift is at the lift value specified in the payload of this command as long as that value is not larger than InstalledOpenLimit - Lift and not smaller than InstalledClosedLimit - Lift.
| #define COMMAND_WINDOW_COVERING_GO_TO_TILT_PERCENTAGE ( 0x08 ) |
Upon receipt of this command, the Window Covering will adjust the window so the physical tilt is at the tilt percentage specified in the payload of this command.
| #define COMMAND_WINDOW_COVERING_GO_TO_TILT_VALUE ( 0x07 ) |
Upon receipt of this command, the Window Covering will adjust the window so the physical tilt is at the tilt value specified in the payload of this command as long as that value is not larger than InstalledOpenLimit - Tilt and not smaller than InstalledClosedLimit - Tilt.
| #define COMMAND_WINDOW_COVERING_STOP ( 0x02 ) |
Upon receipt of this command, the Window Covering will stop any adjusting to the physical tilt and lift that is currently occurring.
| #define COMMAND_WINDOW_COVERING_UP_OR_OPEN ( 0x00 ) |
Upon receipt of this command, the Window Covering will adjust the window so the physical lift is at the InstalledOpenLimit - Lift and the tilt is at the InstalledOpenLimit - Tilt. This will happen as fast as possible.