TI-15.4 Stack API  5.30.00.26
Data Fields
_apimac_securitypibkeyidlookupentry Struct Reference

#include <api_mac.h>

Data Fields

uint16_t keyIndex
 
uint8_t keyIdLookupIndex
 
ApiMac_keyIdLookupDescriptor_t lookupEntry
 

Detailed Description

Security PIB Key ID lookup entry for a Get/Set ApiMac_securityAttribute_keyIdLookupEntry

Field Documentation

§ keyIndex

uint16_t _apimac_securitypibkeyidlookupentry::keyIndex

index into the macKeyIdLookupList

§ keyIdLookupIndex

uint8_t _apimac_securitypibkeyidlookupentry::keyIdLookupIndex

index into macKeyIdLookupList[keyIndex]

§ lookupEntry

ApiMac_keyIdLookupDescriptor_t _apimac_securitypibkeyidlookupentry::lookupEntry

Place to put the requested data


The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale