rflib
Data Fields
rfc_CMD_PROP_TX_s Struct Reference

Proprietary Mode Transmit Command. More...

#include <rf_prop_cmd.h>

Collaboration diagram for rfc_CMD_PROP_TX_s:
Collaboration graph
[legend]

Data Fields

uint16_t commandNo
 The command ID number 0x3801. More...
 
uint16_t status
 An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More...
 
rfc_radioOp_tpNextOp
 Pointer to the next operation to run after this operation is done. More...
 
ratmr_t startTime
 Absolute or relative start time (depending on the value of startTrigger) More...
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
startTrigger
 Identification of the trigger that starts the operation. More...
 
struct {
   uint8_t   rule:4
 Condition for running next command: Rule for how to proceed. More...
 
   uint8_t   nSkip:4
 Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More...
 
condition
 
struct {
   uint8_t   bFsOff:1
 0: Keep frequency synth on after command
1: Turn frequency synth off after command More...
 
   uint8_t   __pad0__:2
 
   uint8_t   bUseCrc:1
 0: Do not append CRC
1: Append CRC More...
 
   uint8_t   bVarLen:1
 0: Fixed length
1: Transmit length as first byte More...
 
pktConf
 
uint8_t pktLen
 Packet length. More...
 
uint32_t syncWord
 Sync word to transmit. More...
 
uint8_t * pPkt
 Pointer to packet. More...
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
startTrigger
 Identification of the trigger that starts the operation. More...
 
struct {
   uint8_t   rule:4
 Condition for running next command: Rule for how to proceed. More...
 
   uint8_t   nSkip:4
 Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More...
 
condition
 
struct {
   uint8_t   bFsOff:1
 0: Keep frequency synth on after command
1: Turn frequency synth off after command More...
 
   uint8_t   __pad0__:2
 
   uint8_t   bUseCrc:1
 0: Do not append CRC
1: Append CRC More...
 
   uint8_t   bVarLen:1
 0: Fixed length
1: Transmit length as first byte More...
 
pktConf
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
startTrigger
 Identification of the trigger that starts the operation. More...
 
struct {
   uint8_t   rule:4
 Condition for running next command: Rule for how to proceed. More...
 
   uint8_t   nSkip:4
 Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More...
 
condition
 
struct {
   uint8_t   bFsOff:1
 0: Keep frequency synth on after command
1: Turn frequency synth off after command More...
 
   uint8_t   __pad0__:2
 
   uint8_t   bUseCrc:1
 0: Do not append CRC
1: Append CRC More...
 
   uint8_t   bVarLen:1
 0: Fixed length
1: Transmit length as first byte More...
 
pktConf
 

Detailed Description

Proprietary Mode Transmit Command.

Field Documentation

§ commandNo

uint16_t rfc_CMD_PROP_TX_s::commandNo

The command ID number 0x3801.

§ status

uint16_t rfc_CMD_PROP_TX_s::status

An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.

§ pNextOp

rfc_radioOp_t * rfc_CMD_PROP_TX_s::pNextOp

Pointer to the next operation to run after this operation is done.

§ startTime

ratmr_t rfc_CMD_PROP_TX_s::startTime

Absolute or relative start time (depending on the value of startTrigger)

§ triggerType

uint8_t rfc_CMD_PROP_TX_s::triggerType

The type of trigger.

§ bEnaCmd

uint8_t rfc_CMD_PROP_TX_s::bEnaCmd

0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger

§ triggerNo

uint8_t rfc_CMD_PROP_TX_s::triggerNo

The trigger number of the CMD_TRIGGER command that triggers this action.

§ pastTrig

uint8_t rfc_CMD_PROP_TX_s::pastTrig

0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible

§ startTrigger [1/3]

struct { ... } rfc_CMD_PROP_TX_s::startTrigger

Identification of the trigger that starts the operation.

§ rule

uint8_t rfc_CMD_PROP_TX_s::rule

Condition for running next command: Rule for how to proceed.

§ nSkip

uint8_t rfc_CMD_PROP_TX_s::nSkip

Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ...

§ condition [1/3]

struct { ... } rfc_CMD_PROP_TX_s::condition

§ bFsOff

uint8_t rfc_CMD_PROP_TX_s::bFsOff

0: Keep frequency synth on after command
1: Turn frequency synth off after command

§ __pad0__

uint8_t rfc_CMD_PROP_TX_s::__pad0__

§ bUseCrc

uint8_t rfc_CMD_PROP_TX_s::bUseCrc

0: Do not append CRC
1: Append CRC

§ bVarLen

uint8_t rfc_CMD_PROP_TX_s::bVarLen

0: Fixed length
1: Transmit length as first byte

§ pktConf [1/3]

struct { ... } rfc_CMD_PROP_TX_s::pktConf

§ pktLen

uint8_t rfc_CMD_PROP_TX_s::pktLen

Packet length.

§ syncWord

uint32_t rfc_CMD_PROP_TX_s::syncWord

Sync word to transmit.

§ pPkt

uint8_t * rfc_CMD_PROP_TX_s::pPkt

Pointer to packet.

§ startTrigger [2/3]

struct { ... } rfc_CMD_PROP_TX_s::startTrigger

Identification of the trigger that starts the operation.

§ condition [2/3]

struct { ... } rfc_CMD_PROP_TX_s::condition

§ pktConf [2/3]

struct { ... } rfc_CMD_PROP_TX_s::pktConf

§ startTrigger [3/3]

struct { ... } rfc_CMD_PROP_TX_s::startTrigger

Identification of the trigger that starts the operation.

§ condition [3/3]

struct { ... } rfc_CMD_PROP_TX_s::condition

§ pktConf [3/3]

struct { ... } rfc_CMD_PROP_TX_s::pktConf

The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale