rflib
Data Fields
rfc_CMD_IEEE_TX_s Struct Reference

IEEE 802.15.4 Transmit Command. More...

#include <rf_ieee_cmd.h>

Collaboration diagram for rfc_CMD_IEEE_TX_s:
Collaboration graph
[legend]

Data Fields

uint16_t commandNo
 The command ID number 0x2C01. More...
 
uint16_t status
 An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More...
 
rfc_radioOp_tpNextOp
 Pointer to the next operation to run after this operation is done. More...
 
ratmr_t startTime
 Absolute or relative start time (depending on the value of startTrigger) More...
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
startTrigger
 Identification of the trigger that starts the operation. More...
 
struct {
   uint8_t   rule:4
 Condition for running next command: Rule for how to proceed. More...
 
   uint8_t   nSkip:4
 Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More...
 
condition
 
struct {
   uint8_t   bIncludePhyHdr:1
 0: Find PHY header automatically
1: Insert PHY header from the buffer More...
 
   uint8_t   bIncludeCrc:1
 0: Append automatically calculated CRC
1: Insert FCS (CRC) from the buffer More...
 
   uint8_t   __pad0__:1
 
   uint8_t   payloadLenMsb:5
 Most significant bits of payload length. Should only be non-zero to create long non-standard packets for test purposes. More...
 
txOpt
 
uint8_t payloadLen
 Number of bytes in the payload. More...
 
uint8_t * pPayload
 Pointer to payload buffer of size payloadLen More...
 
ratmr_t timeStamp
 Time stamp of transmitted frame. More...
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
startTrigger
 Identification of the trigger that starts the operation. More...
 
struct {
   uint8_t   rule:4
 Condition for running next command: Rule for how to proceed. More...
 
   uint8_t   nSkip:4
 Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More...
 
condition
 
struct {
   uint8_t   bIncludePhyHdr:1
 0: Find PHY header automatically
1: Insert PHY header from the buffer More...
 
   uint8_t   bIncludeCrc:1
 0: Append automatically calculated CRC
1: Insert FCS (CRC) from the buffer More...
 
   uint8_t   __pad0__:1
 
   uint8_t   payloadLenMsb:5
 Most significant bits of payload length. Should only be non-zero to create long non-standard packets for test purposes. More...
 
txOpt
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
startTrigger
 Identification of the trigger that starts the operation. More...
 
struct {
   uint8_t   rule:4
 Condition for running next command: Rule for how to proceed. More...
 
   uint8_t   nSkip:4
 Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More...
 
condition
 
struct {
   uint8_t   bIncludePhyHdr:1
 0: Find PHY header automatically
1: Insert PHY header from the buffer More...
 
   uint8_t   bIncludeCrc:1
 0: Append automatically calculated CRC
1: Insert FCS (CRC) from the buffer More...
 
   uint8_t   __pad0__:1
 
   uint8_t   payloadLenMsb:5
 Most significant bits of payload length. Should only be non-zero to create long non-standard packets for test purposes. More...
 
txOpt
 

Detailed Description

IEEE 802.15.4 Transmit Command.

Field Documentation

§ commandNo

uint16_t rfc_CMD_IEEE_TX_s::commandNo

The command ID number 0x2C01.

§ status

uint16_t rfc_CMD_IEEE_TX_s::status

An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.

§ pNextOp

rfc_radioOp_t * rfc_CMD_IEEE_TX_s::pNextOp

Pointer to the next operation to run after this operation is done.

§ startTime

ratmr_t rfc_CMD_IEEE_TX_s::startTime

Absolute or relative start time (depending on the value of startTrigger)

§ triggerType

uint8_t rfc_CMD_IEEE_TX_s::triggerType

The type of trigger.

§ bEnaCmd

uint8_t rfc_CMD_IEEE_TX_s::bEnaCmd

0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger

§ triggerNo

uint8_t rfc_CMD_IEEE_TX_s::triggerNo

The trigger number of the CMD_TRIGGER command that triggers this action.

§ pastTrig

uint8_t rfc_CMD_IEEE_TX_s::pastTrig

0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible

§ startTrigger [1/3]

struct { ... } rfc_CMD_IEEE_TX_s::startTrigger

Identification of the trigger that starts the operation.

§ rule

uint8_t rfc_CMD_IEEE_TX_s::rule

Condition for running next command: Rule for how to proceed.

§ nSkip

uint8_t rfc_CMD_IEEE_TX_s::nSkip

Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ...

§ condition [1/3]

struct { ... } rfc_CMD_IEEE_TX_s::condition

§ bIncludePhyHdr

uint8_t rfc_CMD_IEEE_TX_s::bIncludePhyHdr

0: Find PHY header automatically
1: Insert PHY header from the buffer

§ bIncludeCrc

uint8_t rfc_CMD_IEEE_TX_s::bIncludeCrc

0: Append automatically calculated CRC
1: Insert FCS (CRC) from the buffer

§ __pad0__

uint8_t rfc_CMD_IEEE_TX_s::__pad0__

§ payloadLenMsb

uint8_t rfc_CMD_IEEE_TX_s::payloadLenMsb

Most significant bits of payload length. Should only be non-zero to create long non-standard packets for test purposes.

§ txOpt [1/3]

struct { ... } rfc_CMD_IEEE_TX_s::txOpt

§ payloadLen

uint8_t rfc_CMD_IEEE_TX_s::payloadLen

Number of bytes in the payload.

§ pPayload

uint8_t * rfc_CMD_IEEE_TX_s::pPayload

Pointer to payload buffer of size payloadLen

§ timeStamp

ratmr_t rfc_CMD_IEEE_TX_s::timeStamp

Time stamp of transmitted frame.

§ startTrigger [2/3]

struct { ... } rfc_CMD_IEEE_TX_s::startTrigger

Identification of the trigger that starts the operation.

§ condition [2/3]

struct { ... } rfc_CMD_IEEE_TX_s::condition

§ txOpt [2/3]

struct { ... } rfc_CMD_IEEE_TX_s::txOpt

§ startTrigger [3/3]

struct { ... } rfc_CMD_IEEE_TX_s::startTrigger

Identification of the trigger that starts the operation.

§ condition [3/3]

struct { ... } rfc_CMD_IEEE_TX_s::condition

§ txOpt [3/3]

struct { ... } rfc_CMD_IEEE_TX_s::txOpt

The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale