rflib
Data Fields
rfTrim_t Struct Reference

#include <rfc.h>

Data Fields

uint32_t configIfAdc
 
uint32_t configRfFrontend
 
uint32_t configSynth
 
uint32_t configMiscAdc
 
uint32_t configRfCommon
 
uint8_t loDivider
 
uint8_t noTrim
 

Field Documentation

§ configIfAdc

uint32_t rfTrim_t::configIfAdc

§ configRfFrontend

uint32_t rfTrim_t::configRfFrontend

§ configSynth

uint32_t rfTrim_t::configSynth

§ configMiscAdc

uint32_t rfTrim_t::configMiscAdc

§ configRfCommon

uint32_t rfTrim_t::configRfCommon

§ loDivider

uint8_t rfTrim_t::loDivider

§ noTrim

uint8_t rfTrim_t::noTrim

The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale