Data Fields
KeyStore_PSA_preProvisionedKeyIDs Struct Reference

Structure for storing IDs of pre-provisioned keys. More...

#include <CryptoKeyKeyStore_PSA.h>

Data Fields

uint8_t * addr
 
KeyStore_PSA_KeyFileId id
 
KeyStore_PSA_Algorithm alg
 
KeyStore_PSA_KeyUsage usage
 
uint32_t export
 
uint32_t keyLength
 

Detailed Description

Structure for storing IDs of pre-provisioned keys.

Also stores minimal meta data required to import pre-provisioned keys from persistent memory

Field Documentation

§ addr

uint8_t* KeyStore_PSA_preProvisionedKeyIDs::addr

§ id

KeyStore_PSA_KeyFileId KeyStore_PSA_preProvisionedKeyIDs::id

§ alg

KeyStore_PSA_Algorithm KeyStore_PSA_preProvisionedKeyIDs::alg

§ usage

KeyStore_PSA_KeyUsage KeyStore_PSA_preProvisionedKeyIDs::usage

§ export

uint32_t KeyStore_PSA_preProvisionedKeyIDs::export

§ keyLength

uint32_t KeyStore_PSA_preProvisionedKeyIDs::keyLength

The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale