Data Fields
DACCC26XX_HWAttrs Struct Reference

DACCC26XX Hardware attributes These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. More...

#include <DACCC26X2.h>

Data Fields

uint_least8_t outputPin
 
DAC_VrefSource dacVrefSource
 
uint8_t dacCompAInput
 
bool dacPrecharge
 

Detailed Description

DACCC26XX Hardware attributes These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions.

Field Documentation

§ outputPin

uint_least8_t DACCC26XX_HWAttrs::outputPin

< Pin used for DAC output DAC voltage reference source

§ dacVrefSource

DAC_VrefSource DACCC26XX_HWAttrs::dacVrefSource

Internal signal routed to COMPA_IN

§ dacCompAInput

uint8_t DACCC26XX_HWAttrs::dacCompAInput

Flag to determine precharge state when DCOUPL has been selected as voltage reference

§ dacPrecharge

bool DACCC26XX_HWAttrs::dacPrecharge

The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale