![]() |
![]() |
![]() |
Modules | |
Command Codes | |
Macros | |
#define | ADC_CMD_RESERVED |
#define | ADC_STATUS_RESERVED |
#define | ADC_STATUS_SUCCESS (0) |
Successful status code returned by ADC_control(). More... | |
#define | ADC_STATUS_ERROR (-1) |
Generic error status code returned by ADC_control(). More... | |
#define | ADC_STATUS_UNDEFINEDCMD (-2) |
An error status code returned by ADC_control() for undefined command codes. More... | |
These ADC macros are reservations for ADC.h
#define ADC_CMD_RESERVED |
Common ADC_control command code reservation offset. ADC driver implementations should offset command codes with ADC_CMD_RESERVED growing positively
Example implementation specific command codes:
#define ADC_STATUS_RESERVED |
Common ADC_control status code reservation offset. ADC driver implementations should offset status codes with ADC_STATUS_RESERVED growing negatively.
Example implementation specific status codes:
#define ADC_STATUS_SUCCESS (0) |
Successful status code returned by ADC_control().
ADC_control() returns ADC_STATUS_SUCCESS if the control code was executed successfully.
#define ADC_STATUS_ERROR (-1) |
Generic error status code returned by ADC_control().
ADC_control() returns ADC_STATUS_ERROR if the control code was not executed successfully.
#define ADC_STATUS_UNDEFINEDCMD (-2) |
An error status code returned by ADC_control() for undefined command codes.
ADC_control() returns ADC_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.