![]() |
![]() |
Secure Crypto Service.
The Secure KeyStore driver is used to access all KeyStore functions when using the Secure Processing Environment (SPE).
#include <stdint.h>
#include <ti/drivers/crypto/CryptoCC26X4_s.h>
#include <ti/drivers/cryptoutils/cryptokey/CryptoKeyKeyStore_PSA.h>
#include <third_party/tfm/interface/include/psa/crypto.h>
#include <third_party/tfm/interface/include/psa/service.h>
#include <third_party/tfm/interface/include/psa/crypto_client_struct.h>
Go to the source code of this file.
Data Structures | |
struct | KeyStore_s_GetKeyMsg |
struct | KeyStore_s_GenerateKeyMsg |
struct | KeyStore_s_ExportMsg |
struct | KeyStore_s_ImportCertificateMsg |
struct | KeyStore_s_ImportKeyMsg |
struct | KeyStore_s_DestroyPurgeKeyCertificateMsg |
struct | KeyStore_s_GetKeyAttributesMsg |
struct | KeyStore_s_ResetKeyAttributesMsg |
Functions | |
psa_status_t | KeyStore_s_handlePsaMsg (psa_msg_t *msg) |
Handles PSA messages for KeyStore secure driver. More... | |
void | KeyStore_s_init (void) |
Initializes the KeyStore secure driver. More... | |
psa_status_t | KeyStore_s_copyKeyAttributesFromClient (struct psa_client_key_attributes_s *clientKeyAttr, int32_t clientId, psa_key_attributes_t *keyAttributes) |
Gets key attributes from client key attributes. Follows tfm_crypto_key_attributes_from_client() More... | |
void | KeyStore_s_copyKeyIDFromClient (KeyStore_PSA_KeyFileId *keyID, int32_t clientId, uint32_t *clientKeyID) |
Copies client key ID from non-secure side to secure side. More... | |
#define KEYSTORE_PSA_S_MSG_CALC | ( | a | ) | (CRYPTO_S_MSG_TYPE_INDEX_KEYSTORE | ((int32_t)1 << (CRYPTO_S_MSG_TYPE_SHIFT + a))) |
#define KEYSTORE_PSA_S_MSG_TYPE_GET_KEY KEYSTORE_PSA_S_MSG_CALC(0U) |
#define KEYSTORE_PSA_S_MSG_TYPE_GENERATE_KEY KEYSTORE_PSA_S_MSG_CALC(1U) |
#define KEYSTORE_PSA_S_MSG_TYPE_EXPORT_CERTIFICATE KEYSTORE_PSA_S_MSG_CALC(2U) |
#define KEYSTORE_PSA_S_MSG_TYPE_EXPORT_PUBLIC_KEY KEYSTORE_PSA_S_MSG_CALC(3U) |
#define KEYSTORE_PSA_S_MSG_TYPE_EXPORT_KEY KEYSTORE_PSA_S_MSG_CALC(4U) |
#define KEYSTORE_PSA_S_MSG_TYPE_DESTROY_CERTIFICATE KEYSTORE_PSA_S_MSG_CALC(5U) |
#define KEYSTORE_PSA_S_MSG_TYPE_DESTROY_KEY KEYSTORE_PSA_S_MSG_CALC(6U) |
#define KEYSTORE_PSA_S_MSG_TYPE_IMPORT_CERTIFICATE KEYSTORE_PSA_S_MSG_CALC(7U) |
#define KEYSTORE_PSA_S_MSG_TYPE_IMPORT_KEY KEYSTORE_PSA_S_MSG_CALC(8U) |
#define KEYSTORE_PSA_S_MSG_TYPE_PURGE_KEY KEYSTORE_PSA_S_MSG_CALC(9U) |
#define KEYSTORE_PSA_S_MSG_TYPE_GET_KEY_ATTRIBUTES KEYSTORE_PSA_S_MSG_CALC(10U) |
#define KEYSTORE_PSA_S_MSG_TYPE_RESET_KEY_ATTRIBUTES KEYSTORE_PSA_S_MSG_CALC(11U) |
psa_status_t KeyStore_s_handlePsaMsg | ( | psa_msg_t * | msg | ) |
Handles PSA messages for KeyStore secure driver.
[in] | msg | pointer to PSA message |
PSA_SUCCESS | if successful. |
PSA_ERROR_PROGRAMMER_ERROR | if any args point to secure addresses. |
void KeyStore_s_init | ( | void | ) |
Initializes the KeyStore secure driver.
psa_status_t KeyStore_s_copyKeyAttributesFromClient | ( | struct psa_client_key_attributes_s * | clientKeyAttr, |
int32_t | clientId, | ||
psa_key_attributes_t * | keyAttributes | ||
) |
Gets key attributes from client key attributes. Follows tfm_crypto_key_attributes_from_client()
[in] | clientKeyAttr | Client key attributes, address location must be verified to be in non-secure memory by calling functions |
[in] | clientId | Partition ID of the calling client |
[out] | keyAttributes | Key attributes, no address verification necessary as this is always in secure side |
void KeyStore_s_copyKeyIDFromClient | ( | KeyStore_PSA_KeyFileId * | keyID, |
int32_t | clientId, | ||
uint32_t * | clientKeyID | ||
) |
Copies client key ID from non-secure side to secure side.
[out] | keyID | Key ID, no address verification necessary as this is always in secure side |
[in] | clientKeyID | Client key ID, address location must be verified to be in non-secure memory by calling functions |
[in] | clientId | Client ID, partition ID from PSA call |