CC26xx Driver Library
pka.h File Reference
#include "../inc/hw_types.h"
#include "../inc/hw_memmap.h"
#include "../inc/hw_ints.h"
#include "../inc/hw_pka.h"
#include "../inc/hw_pka_ram.h"
#include "interrupt.h"
#include "sys_ctrl.h"
#include "debug.h"
#include <string.h>

Data Structures

union  PKA_EccParam224
 
union  PKA_EccParam256
 
union  PKA_EccParam384
 
union  PKA_EccParam512
 
union  PKA_EccParam521
 
struct  PKA_EccPoint224_
 
struct  PKA_EccPoint256_
 
struct  PKA_EccPoint384_
 
struct  PKA_EccPoint512_
 
struct  PKA_EccPoint521_
 

Macros

#define PKA_STATUS_SUCCESS   0
 Success. More...
 
#define PKA_STATUS_FAILURE   1
 Failure. More...
 
#define PKA_STATUS_INVALID_PARAM   2
 Invalid parameter. More...
 
#define PKA_STATUS_BUF_UNDERFLOW   3
 Buffer underflow. More...
 
#define PKA_STATUS_RESULT_0   4
 Result is all zeros. More...
 
#define PKA_STATUS_A_GREATER_THAN_B   5
 Big number compare return status if the first big number is greater than the second. More...
 
#define PKA_STATUS_A_LESS_THAN_B   6
 Big number compare return status if the first big number is less than the second. More...
 
#define PKA_STATUS_EQUAL   7
 Big number compare return status if the first big number is equal to the second. More...
 
#define PKA_STATUS_OPERATION_BUSY   8
 PKA operation is in progress. More...
 
#define PKA_STATUS_OPERATION_RDY   9
 No PKA operation is in progress. More...
 
#define PKA_STATUS_LOCATION_IN_USE   10
 Location in PKA RAM is not available. More...
 
#define PKA_STATUS_X_ZERO   11
 X coordinate of public key is 0. More...
 
#define PKA_STATUS_Y_ZERO   12
 Y coordinate of public key is 0. More...
 
#define PKA_STATUS_X_LARGER_THAN_PRIME   13
 X coordinate of public key is larger than the curve prime. More...
 
#define PKA_STATUS_Y_LARGER_THAN_PRIME   14
 Y coordinate of public key is larger than the curve prime. More...
 
#define PKA_STATUS_POINT_NOT_ON_CURVE   15
 The public key is not on the specified elliptic curve. More...
 
#define PKA_STATUS_RESULT_ADDRESS_INCORRECT   16
 The address of the result passed into one of the PKA*GetResult functions is incorrect. More...
 
#define PKA_STATUS_POINT_AT_INFINITY   17
 The ECC operation resulted in the point at infinity. More...
 
#define NISTP224_PARAM_SIZE_BYTES   28
 
#define NISTP256_PARAM_SIZE_BYTES   32
 
#define NISTP384_PARAM_SIZE_BYTES   48
 
#define NISTP521_PARAM_SIZE_BYTES   66
 
#define BrainpoolP256R1_PARAM_SIZE_BYTES   32
 
#define BrainpoolP384R1_PARAM_SIZE_BYTES   48
 
#define BrainpoolP512R1_PARAM_SIZE_BYTES   64
 
#define Curve25519_PARAM_SIZE_BYTES   32
 

Typedefs

typedef struct PKA_EccPoint224_ PKA_EccPoint224
 
typedef struct PKA_EccPoint256_ PKA_EccPoint256
 
typedef struct PKA_EccPoint384_ PKA_EccPoint384
 
typedef struct PKA_EccPoint512_ PKA_EccPoint512
 
typedef struct PKA_EccPoint521_ PKA_EccPoint521
 

Functions

void PKAClearPkaRam (void)
 Zeroizes PKA RAM. More...
 
uint32_t PKAGetOpsStatus (void)
 Gets the PKA operation status. More...
 
bool PKAArrayAllZeros (const uint8_t *array, uint32_t arrayLength)
 Checks whether and array only consists of zeros. More...
 
void PKAZeroOutArray (const uint8_t *array, uint32_t arrayLength)
 Zeros-out an array. More...
 
uint32_t PKABigNumModStart (const uint8_t *bigNum, uint32_t bigNumLength, const uint8_t *modulus, uint32_t modulusLength, uint32_t *resultPKAMemAddr)
 Starts a big number modulus operation. More...
 
uint32_t PKABigNumModGetResult (uint8_t *resultBuf, uint32_t length, uint32_t resultPKAMemAddr)
 Gets the result of the big number modulus operation. More...
 
uint32_t PKABigNumDivideStart (const uint8_t *dividend, uint32_t dividendLength, const uint8_t *divisor, uint32_t divisorLength, uint32_t *resultQuotientMemAddr, uint32_t *resultRemainderMemAddr)
 Starts a big number divide operation. More...
 
uint32_t PKABigNumDivideGetQuotient (uint8_t *resultBuf, uint32_t *length, uint32_t resultQuotientMemAddr)
 Gets the quotient of the big number divide operation. More...
 
uint32_t PKABigNumDivideGetRemainder (uint8_t *resultBuf, uint32_t *length, uint32_t resultRemainderMemAddr)
 Gets the remainder of the big number divide operation. More...
 
uint32_t PKABigNumCmpStart (const uint8_t *bigNum1, const uint8_t *bigNum2, uint32_t length)
 Starts the comparison of two big numbers. More...
 
uint32_t PKABigNumCmpGetResult (void)
 Gets the result of the comparison operation of two big numbers. More...
 
uint32_t PKABigNumInvModStart (const uint8_t *bigNum, uint32_t bigNumLength, const uint8_t *modulus, uint32_t modulusLength, uint32_t *resultPKAMemAddr)
 Starts a big number inverse modulo operation. More...
 
uint32_t PKABigNumInvModGetResult (uint8_t *resultBuf, uint32_t length, uint32_t resultPKAMemAddr)
 Gets the result of the big number inverse modulo operation. More...
 
uint32_t PKABigNumExpModStart (const uint8_t *base, uint32_t baseLength, const uint8_t *exponent, uint32_t exponentLength, const uint8_t *modulus, uint32_t modulusLength, uint32_t *resultPKAMemAddr)
 Starts a big number modular exponentiation operation. More...
 
uint32_t PKABigNumExpModGetResult (uint8_t *resultBuf, uint32_t length, uint32_t resultPKAMemAddr)
 Gets the result of the big number modular exponentiation operation. More...
 
uint32_t PKABigNumMultiplyStart (const uint8_t *multiplicand, uint32_t multiplicandLength, const uint8_t *multiplier, uint32_t multiplierLength, uint32_t *resultPKAMemAddr)
 Starts the multiplication of two big numbers. More...
 
uint32_t PKABigNumMultGetResult (uint8_t *resultBuf, uint32_t *resultLength, uint32_t resultPKAMemAddr)
 Gets the result of the big number multiplication. More...
 
uint32_t PKABigNumAddStart (const uint8_t *bigNum1, uint32_t bigNum1Length, const uint8_t *bigNum2, uint32_t bigNum2Length, uint32_t *resultPKAMemAddr)
 Starts the addition of two big numbers. More...
 
uint32_t PKABigNumAddGetResult (uint8_t *resultBuf, uint32_t *resultLength, uint32_t resultPKAMemAddr)
 Gets the result of the addition operation on two big numbers. More...
 
uint32_t PKABigNumSubStart (const uint8_t *minuend, uint32_t minuendLength, const uint8_t *subtrahend, uint32_t subtrahendLength, uint32_t *resultPKAMemAddr)
 Starts the subtraction of one big number from another. More...
 
uint32_t PKABigNumSubGetResult (uint8_t *resultBuf, uint32_t *resultLength, uint32_t resultPKAMemAddr)
 Gets the result of the subtraction operation on two big numbers. More...
 
uint32_t PKAEccMultiplyStart (const uint8_t *scalar, const uint8_t *curvePointX, const uint8_t *curvePointY, const uint8_t *prime, const uint8_t *a, const uint8_t *b, uint32_t length, uint32_t *resultPKAMemAddr)
 Starts ECC multiplication. More...
 
uint32_t PKAEccMontgomeryMultiplyStart (const uint8_t *scalar, const uint8_t *curvePointX, const uint8_t *prime, const uint8_t *a, uint32_t length, uint32_t *resultPKAMemAddr)
 Starts ECC Montgomery multiplication. More...
 
uint32_t PKAEccMultiplyGetResult (uint8_t *curvePointX, uint8_t *curvePointY, uint32_t resultPKAMemAddr, uint32_t length)
 Gets the result of ECC multiplication. More...
 
uint32_t PKAEccAddStart (const uint8_t *curvePoint1X, const uint8_t *curvePoint1Y, const uint8_t *curvePoint2X, const uint8_t *curvePoint2Y, const uint8_t *prime, const uint8_t *a, uint32_t length, uint32_t *resultPKAMemAddr)
 Starts the ECC addition. More...
 
uint32_t PKAEccAddGetResult (uint8_t *curvePointX, uint8_t *curvePointY, uint32_t resultPKAMemAddr, uint32_t length)
 Gets the result of the ECC addition. More...
 
uint32_t PKAEccVerifyPublicKeyWeierstrassStart (const uint8_t *curvePointX, const uint8_t *curvePointY, const uint8_t *prime, const uint8_t *a, const uint8_t *b, const uint8_t *order, uint32_t length)
 Begins the validation of a public key against a Short-Weierstrass curve. More...
 

Variables

const PKA_EccPoint224 NISTP224_generator
 X coordinate of the generator point of the NISTP224 curve. More...
 
const PKA_EccParam224 NISTP224_prime
 Prime of the NISTP224 curve. More...
 
const PKA_EccParam224 NISTP224_a
 a constant of the NISTP224 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b). More...
 
const PKA_EccParam224 NISTP224_b
 b constant of the NISTP224 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b). More...
 
const PKA_EccParam224 NISTP224_order
 Order of the NISTP224 curve. More...
 
const PKA_EccPoint256 NISTP256_generator
 X coordinate of the generator point of the NISTP256 curve. More...
 
const PKA_EccParam256 NISTP256_prime
 Prime of the NISTP256 curve. More...
 
const PKA_EccParam256 NISTP256_a
 a constant of the NISTP256 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b). More...
 
const PKA_EccParam256 NISTP256_b
 b constant of the NISTP256 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b). More...
 
const PKA_EccParam256 NISTP256_order
 Order of the NISTP256 curve. More...
 
const PKA_EccPoint384 NISTP384_generator
 X coordinate of the generator point of the NISTP384 curve. More...
 
const PKA_EccParam384 NISTP384_prime
 Prime of the NISTP384 curve. More...
 
const PKA_EccParam384 NISTP384_a
 a constant of the NISTP384 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b). More...
 
const PKA_EccParam384 NISTP384_b
 b constant of the NISTP384 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b). More...
 
const PKA_EccParam384 NISTP384_order
 Order of the NISTP384 curve. More...
 
const PKA_EccPoint521 NISTP521_generator
 X coordinate of the generator point of the NISTP521 curve. More...
 
const PKA_EccParam521 NISTP521_prime
 Prime of the NISTP521 curve. More...
 
const PKA_EccParam521 NISTP521_a
 a constant of the NISTP521 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b). More...
 
const PKA_EccParam521 NISTP521_b
 b constant of the NISTP521 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b). More...
 
const PKA_EccParam521 NISTP521_order
 Order of the NISTP521 curve. More...
 
const PKA_EccPoint256 BrainpoolP256R1_generator
 X coordinate of the generator point of the BrainpoolP256R1 curve. More...
 
const PKA_EccParam256 BrainpoolP256R1_prime
 Prime of the BrainpoolP256R1 curve. More...
 
const PKA_EccParam256 BrainpoolP256R1_a
 a constant of the BrainpoolP256R1 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b). More...
 
const PKA_EccParam256 BrainpoolP256R1_b
 b constant of the BrainpoolP256R1 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b). More...
 
const PKA_EccParam256 BrainpoolP256R1_order
 Order of the BrainpoolP256R1 curve. More...
 
const PKA_EccPoint384 BrainpoolP384R1_generator
 X coordinate of the generator point of the BrainpoolP384R1 curve. More...
 
const PKA_EccParam384 BrainpoolP384R1_prime
 Prime of the BrainpoolP384R1 curve. More...
 
const PKA_EccParam384 BrainpoolP384R1_a
 a constant of the BrainpoolP384R1 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b). More...
 
const PKA_EccParam384 BrainpoolP384R1_b
 b constant of the BrainpoolP384R1 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b). More...
 
const PKA_EccParam384 BrainpoolP384R1_order
 Order of the BrainpoolP384R1 curve. More...
 
const PKA_EccPoint512 BrainpoolP512R1_generator
 X coordinate of the generator point of the BrainpoolP512R1 curve. More...
 
const PKA_EccParam512 BrainpoolP512R1_prime
 Prime of the BrainpoolP512R1 curve. More...
 
const PKA_EccParam512 BrainpoolP512R1_a
 a constant of the BrainpoolP512R1 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b). More...
 
const PKA_EccParam512 BrainpoolP512R1_b
 b constant of the BrainpoolP512R1 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b). More...
 
const PKA_EccParam512 BrainpoolP512R1_order
 Order of the BrainpoolP512R1 curve. More...
 
const PKA_EccPoint256 Curve25519_generator
 X coordinate of the generator point of the Curve25519 curve. More...
 
const PKA_EccParam256 Curve25519_prime
 Prime of the Curve25519 curve. More...
 
const PKA_EccParam256 Curve25519_a
 a constant of the Curve25519 curve when expressed in Montgomery form (By^2 = x^3 + a*x^2 + x). More...
 
const PKA_EccParam256 Curve25519_b
 b constant of the Curve25519 curve when expressed in Montgomery form (By^2 = x^3 + a*x^2 + x). More...
 
const PKA_EccParam256 Curve25519_order
 Order of the Curve25519 curve. More...