CC26xx Driver Library
aon_pmctl.h File Reference
#include <stdbool.h>
#include <stdint.h>
#include "../inc/hw_types.h"
#include "../inc/hw_memmap.h"
#include "../inc/hw_memmap_common.h"
#include "../inc/hw_aon_pmctl.h"
#include "debug.h"

Macros

#define MCU_RAM_RET_NONE   AON_PMCTL_RAMCFG_BUS_SRAM_RET_EN_RET_NONE
 
#define MCU_RAM_RET_LVL1   AON_PMCTL_RAMCFG_BUS_SRAM_RET_EN_RET_LEVEL1
 
#define MCU_RAM_RET_LVL2   AON_PMCTL_RAMCFG_BUS_SRAM_RET_EN_RET_LEVEL2
 
#define MCU_RAM_RET_LVL3   AON_PMCTL_RAMCFG_BUS_SRAM_RET_EN_RET_LEVEL3
 
#define MCU_RAM_RET_FULL   AON_PMCTL_RAMCFG_BUS_SRAM_RET_EN_RET_FULL
 
#define AONPMCTL_JTAG_POWER_ON   AON_PMCTL_PWRSTAT_JTAG_PD_ON
 

Functions

static void AONPMCTLMcuSRamRetConfig (uint32_t ui32Retention)
 Configure the retention on the block SRAM in the MCU BUS domain. More...
 
static uint32_t AONPMCTLPowerStatusGet (void)
 Get the power status of the Always On (AON) domain. More...
 
static void AONPMCTLJtagPowerOff (void)
 Request power off of the JTAG domain. More...