CC26xx Driver Library
tDMAControlTable Struct Reference

A structure that defines an entry in the channel control table. More...

#include <udma.h>

Data Fields

volatile void * pvSrcEndAddr
 The ending source address of the data transfer. More...
 
volatile void * pvDstEndAddr
 The ending destination address of the data transfer. More...
 
volatile uint32_t ui32Control
 The channel control mode. More...
 
volatile uint32_t ui32Spare
 An unused location. More...
 

Detailed Description

A structure that defines an entry in the channel control table.

These fields are used by the uDMA controller and normally it is not necessary for software to directly read or write fields in the table.

Field Documentation

§ pvDstEndAddr

volatile void* tDMAControlTable::pvDstEndAddr

The ending destination address of the data transfer.

Referenced by uDMAChannelScatterGatherSet(), and uDMAChannelTransferSet().

§ pvSrcEndAddr

volatile void* tDMAControlTable::pvSrcEndAddr

The ending source address of the data transfer.

Referenced by uDMAChannelScatterGatherSet(), and uDMAChannelTransferSet().

§ ui32Control

volatile uint32_t tDMAControlTable::ui32Control

§ ui32Spare

volatile uint32_t tDMAControlTable::ui32Spare

An unused location.

Referenced by uDMAChannelScatterGatherSet().