TI OAD API Documentation  2.02.07.00
Data Fields
securityInfoSeg_t Struct Reference

Data Fields

eccSignature_t eccSign
 Security signature */.
 
uint32_t secSegLen
 Payload segment length.
 
uint8_t secSignerInfo [8]
 Security signer info */.
 
uint32_t secTimestamp
 Security timestamp */.
 
uint8_t secVer
 Security version */.
 
uint8_t segTypeSecure
 Segment type - for Secuirty info payload.
 
uint8_t verifStat
 Verification status.
 
uint16_t wirelessTech
 Wireless technology type.
 

Detailed Description

OAD continuous image payload segment

This segment is used to describe a contiguous region of an image The code data in this blob will be flashed to sequential addresses


The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale