TI OAD API Documentation  2.02.07.00
Data Fields
imgPayloadSeg_t Struct Reference

Data Fields

uint32_t imgSegLen
 Payload segment length.
 
uint8_t rfu
 Reserved byte.
 
uint8_t segTypeImg
 Segment type - for Contiguous image payload.
 
uint32_t startAddr
 Start address of image on internal flash.
 
uint16_t wirelessTech
 Wireless technology type.
 

Detailed Description

OAD continuous image payload segment

This segment is used to describe a contiguous region of an image The code data in this blob will be flashed to sequential addresses


The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale