TI OAD API Documentation  2.02.07.00
Data Fields
boundarySeg_t Struct Reference

Data Fields

uint32_t boundarySegLen
 Boundary segment length.
 
uint32_t ram0EndAddr
 RAM entry end address.
 
uint32_t ram0StartAddr
 RAM entry start address.
 
uint8_t rfu
 Reserved byte.
 
uint8_t segTypeBd
 Segment type - for boundary segment.
 
uint32_t stackEntryAddr
 Stack start address.
 
uint32_t stackStartAddr
 Start address of stack image on internal flash.
 
uint16_t wirelessTech
 Wireless technology type.
 

Detailed Description

OAD boundary segment

This segment is used to describe the RAM and Flash boundaries in a split image system.

Note
This segment is optional and not required if app and stack are linked together as one image.

The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale