TI BLE5-Stack API Documentation  2.02.07.00
Data Fields
rtlsSrv_antennaInfo_t Struct Reference

LE CTE Antenna Information Event RTLSSRV_ANTENNA_INFORMATION_EVT. More...

Data Fields

uint8_t maxCteLen
 maximum cte length supported by the controller
 
uint8_t maxNumOfAntennas
 maximum number of antennas supported by the controller
 
uint8_t maxSwitchPatternLen
 maximum size of switch pattern supported by the controller
 
uint8_t sampleRates
 sample rates supported by the controller
 

Detailed Description

LE CTE Antenna Information Event RTLSSRV_ANTENNA_INFORMATION_EVT.


The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale