TI BLE5-Stack API Documentation  2.02.07.00
Data Fields
hciEvt_BLERemoteConnParamReq_t Struct Reference

LE Remote Connection Parameter Request Event. More...

Data Fields

uint8 BLEEventCode
 BLE Event Code.
 
uint16 connHandle
 connection handle
 
osal_event_hdr_t hdr
 osal event header
 
uint16 Interval_Max
 maximum connection interval
 
uint16 Interval_Min
 minimum connection interval
 
uint16 Latency
 slave latency
 
uint8 status
 status of event
 
uint16 Timeout
 supervision timeout
 

Detailed Description

LE Remote Connection Parameter Request Event.


The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale